Introduction
| Author: Cristian Pop, Microchip Technology Inc. |
The Configurable Custom Logic (CCL) is a programmable logic peripheral that allows the on-chip creation of the logic functions for Microchip tinyAVR® 0- and 1-series, megaAVR® 0-series, and AVR® DA devices. The CCL provides programmable, combinational and sequential logic that operates independently of the CPU execution. It can be connected to a wide range of internal and external inputs such as device pins, events, or other internal peripherals and can serve as a “glue logic” between the device peripherals and external devices.
This technical brief explains how to use the CCL to implement the following functions:
- Logic AND
Gate:
Uses CCL to implement a simple logic AND gate.
- State
Decoder:
Shows how to use CCL combinational logic to detect a specific state of the external signals.
- SR
Latch:
Uses internal CCL sequential logic to create an SR latch.