18.3.1 maxView vSphere Plugin Resources

The following section describes the controller details of the maxView vSphere plugin.

The controller has the following four tabs:

  • Getting Started
  • Summary
  • Device Alert

  • More Objects (VMware specific)

Getting Started Tab

The following figure shows the Getting Started tab that displays the basic information of a controller.

Summary Tab

The Summary tab displays the status and the properties of the controller.

Device Alert Tab

The Device Alert tab display the information(s), warning(s), and errors(s) of the controller.

More Objects Tab

The More Objects tab is a VMware specific tab, which displays the related resources of the controller.

Note:

You can also obtain the similar details of an Array, Enclosure, Event, Logical Device, and Physical device by clicking on the respective tabs.