12.3.3 Locating SSDs in the maxCache Device
To locate the Solid State Drives (SSDs) in the maxCache Device:
- In the Enterprise View, select a controller; then select the maxCache Device on that controller. You can select the maxCache array or logical device.
-
On the ribbon, in the maxCache group, click
Locate.
The Locate maxCache window opens, displaying a list SSDs comprising the maxCache Device.
- Select the time-out period from the drop-down list: 1 hour, 4 hours, 24 hours.
-
Click the Locate button.
The LEDs on the SSDs begin to flash.
- Click Stop to stop blinking the SSDs.
- Click Cancel to close the Locate maxCache window.