13.4 Changing an Operating System's Event Log Setting
In addition to the maxView Storage Manager event log, all Warning- and Error-level events on a system are recorded in its operating system event log. You can select the type of events that are recorded, or you can disable operating system event logging.
Note: This setting is not applicable for ESXi operating system.
To change or disable operating system event logging on a system:
- Select the Enterprise View node.
-
On the ribbon, in the System group, click System
Settings.
The System Settings window opens.
-
In the Save Events to OS Log drop-down list, select the type of
events that you want to log, then click
OK.
- Restart maxView Storage Manager to apply the new setting.