12.9 Setting the Physical Drive Boot Priority
Use this option to set the boot priority of a physical device to Primary, Secondary, Primary and Secondary, or None (default). A controller can have only one physical (or logical) device as the primary or secondary boot device. When you select a new physical device as the primary/secondary boot drive, the boot priority of the existing primary/secondary boot drive is overwritten and set to None.
- In the Enterprise View, select a controller, then select a physical drive on the controller.
-
On the ribbon, in the Physical Device group, click Set
Properties.The Set Properties window opens.
- From the Boot Type drop-down list, select Primary, Secondary, Primary and Secondary, or None.
- Click OK.