12.6.2 Setting a Disk Drive to ‘Failed’
Before you can remove a disk drive, you should set it to the Failed state to protect your data. To fail a disk drive (or SSD), use the Force Offline option for physical devices.
You can set a disk drive to the Failed state if:- The disk drive is not part of a logical drive, or
- The disk drive is part of a redundant, healthy logical drive
Once you force a drive offline, it can be brought online again only after power-cycling the controller.
CAUTION: You may
lose data or damage your disk drive if you remove a disk drive without
first setting it to a failed state.
To set a disk drive to Failed:
- In the Enterprise View, select a controller then, in the Physical Devices tree, select the drive you want to set to Failed.
-
On the ribbon, in the Physical Devices group, click
Force Offline.
The Force Offline window opens.
-
Click Force.
The drive is taken offline and set to the Failed state.
Note: If the drive is part of a healthy logical drive, the drive is degraded and a warning message is displayed in the Event Log.