18.1 Installing the maxView Plugin for vSphere 7 HTML5 Client
Follow the instructions in this section to install the maxView vSphere Plugin HTML5 on a vCenter Server Appliance.
VMware ESXi 7 and vCenter Server Appliance (VCSA) 7 versions are required to be running on the machine before proceeding with the installation steps.
- Create an ESXi setup and mount the
VCSA.iso
file on a machine. - Navigate to the following directory on the mounted file:
\vcsa-ui-installer\win32\installer.exe
- Double-click on the installer and follow the instructions to create a virtual machine in the ESXi machine with the VMware Photon OS.
- Perform either of the following two steps to install the maxView vSphere plugin:
- Download and install the maxView vSphere plugin from the Web site.
- Install the
maxView-plugin.zip
locally by coping the downloadedmaxView-plugin.zip
in/etc/vmware-vpx/locale/ maxView-plugin.zip
.
- Execute the following steps to install the
maxView vSphere plugin.
- Extract the vsphere-client-sdk-7.zip provided by the VMware.
- Navigate to
\html-client-sdk\tools\vCenter plugin registration\prebuilt\
location that contains the plugin registration script. - Run the following command to
register the plugin from the Windows machine:
- Using Microchip Web URL (download.adaptec.com/raid/storage_manager/maxView-plugin.zip):
extension-registration.bat -action registerPlugin --key com.pmc.maxview.maxviewvsphere -url https://IP_ADDRESS/sdk --username Username --version 1.0.0 --vcenterServerThumbprint vcenterServerThumbprint --pluginUrl https://download.adaptec.com/raid/storage_manager/maxView-plugin.zip –serverThumbprint serverThumbprint
- Installing the
maxView-plugin.zip locally:
extension-registration.bat -action registerPlugin --key com.pmc.maxview.maxviewvsphere -url https://IP_ADDRESS/sdk --username Username --version 1.0.0 --vcenterServerThumbprint vcenterServerThumbprint --pluginUrl https:// IP_ADDRESS /catalog/maxView-plugin.zip –serverThumbprint serverThumbprint
Note: For more detail on the commands, check with VMware.
where:IP_Address
is the IP address of the vCenter Server ApplianceUsername
is the username of the vCenter Server Appliance-
vcenterServerThumbprint
is the vCenter Server Appliance SHA1 Thumbprint. To retrieve SHA1 Thumbprint, perform the following steps:- Launch the vCenter Server appliance in the Web browser.
- Click the Lock icon on the address bar to get the certificate.
- View the SHA1
Thumbprint on the certificate.Note: Check the JDK version. vCenter Server Appliance (VCSA) requires JDK 8 to run the plugin.
- The maxView plugin is placed
either at download.adaptec.com/raid/storage_manager/maxView-plugin.zip or, you can use the IP address of the
machine where the
maxView_plugin.zip
is placed. serverThumbprint
is required from the Microchip website.
A password is prompted. Enter the password of the vCenter Server Appliance.
- Using Microchip Web URL (download.adaptec.com/raid/storage_manager/maxView-plugin.zip):
- Run the following command to
de-register the plugin from Windows
machine.
extension-registration.bat -action unregisterPlugin --key com.pmc.maxview.maxviewvsphere -url https://IP_ADDRESS /sdk --username Username --vcenterServerThumbprint vcenterServerThumbprint
Note: For more detail on the commands, check with VMware.where:IP_Address
is the IP address of the vCenter Server ApplianceUsername
is the username of the vCenter Server Appliance-
vcenterServerThumbprint
is the vCenter Server Appliance SHA1 Thumbprint. Retrieve the SHA1 Thumbprint certificate as described in the preceeding step.
A password is prompted. Enter the password of vCenter Server Appliance.
Once the maxView vSphere plugin is registered, the maxView icon is displayed in shortcut of vCenter Server Appliance (https://VCSA_IP/ui/app/shortcuts).
- Click on the maxView icon to list the ESXi systems added.Note: Initially, none of the system are added.
- Click on Add system to add the ESXi systems.
- Add the firewall entry by using URL:
https://VCSA_IP: 5480. Click on the firewall and add the entry.Note: Replace VCSA_IP with the user installed vCenter Server Appliance IP address.Note: The configuration or events are not delivered, if the firewall is not added.