13.3.2 Sending a Test Message
To ensure that an email recipient is receiving event notifications, you can send them a test message.
To send a test message:
- Select the Enterprise View node.
- On the ribbon, in the System group, click System Settings.
-
When the System settings window opens, click the
Email tab.
The Email Notifications Manager opens.
- Select one or more email addresses to send a test message to. To select all addresses, click the check box at the top of the list, as shown in the figure below.
-
Click Send Test Email.
If the test is successful, the email recipient(s) receive the test message. If the test fails:
- Ensure that the recipient's email address is correct. (See 13.3.3 Modifying or Removing an Email Recipient .)
- Ensure that your SMTP server address is correct. (See 13.3.4 Modifying Email Server Settings.)
- Try sending the test message again.