19.1 Installing the maxView Plugin for vSphere 8 HTML5 Client
Follow the instructions in this section to install the maxView vSphere 8 Plugin HTML5 on a vCenter Server Appliance.
- Create an ESXi setup and mount
the
VCSA.iso
file on a machine. - Navigate to the following
directory on the mounted file:
\vcsa-ui-installer\win32\installer.exe
. - Double-click on the installer and follow the instructions to create a virtual machine in the ESXi machine with the VMware Photon OS.
- Perform the following steps to
install the maxView vSphere plugin:
- Copy
maxview-plugin-1.0.0.jar
andmaxview_plugin_Installation.sh
to vCenter Server - Run the
maxview_plugin_Installation.sh
from the same location and provide the following information:vCenter Server GUID
: To retrieve vCenter Server GUID, perform the following steps:- Login to vCenter Server appliance.
- Navigate
to the inventory and copy the GUID from the URL. See the
following figure to retrieve vCenter Server GUID from
the URL:
vCenter Server FQDN
: IP address of the vCenter Server AppliancevCenter Server Thumbprint
: The vCenter Server Appliance SHA1 Thumbprint. See Retrieve SHA1 Thumbprint to retrieve SHA1 Thumbprint.
- Copy
- Execute the following steps to
install the maxView vSphere plugin.
- Navigate to
\html-client-sdk\tools\vCenter plugin registration\prebuilt\
location that contains the plugin registration script. - Run the following command
to register the plugin from the Windows
machine
extension-registration.bat -action registerPlugin -remote -url https:// IP_Address /sdk -username Username -password Password --vcenterServerThumbprint vcenterServerThumbprint -key com.mchp.maxview.maxviewvsphere -version 1.0.0 -pluginUrl https:// IP_Address:8443/maxView-ui/plugin.json -serverThumbprint ServerThumbprint -c "2023 Microchip Technology Inc." -n "maxView Remote Plugin" -s "This is maxView Remote Plugin"
Note: For more detail on the commands, check with VMware.where:-
IP_Address
is the IP address of the vCenter Server Appliance -
Username
is the username of the vCenter Server Appliance -
Password
is the password of the vCenter Server Appliance -
vcenterServerThumbprint
is the vCenter Server Appliance SHA1 ThumbprintNote: ServerThumbprint is the SHA256 Thumbprint of https:// IP_Address:8443/maxView-ui/plugin.json.
-
- Run the following command
to de-register the plugin from Windows
machine.
extension-registration.bat -action unregisterPlugin --key com.pmc.maxview.maxviewvsphere -url https://IP_ADDRESS /sdk --username Username --vcenterServerThumbprint vcenterServerThumbprint
Note: For more detail on the commands, check with VMware.where:-
IP_Address
is the IP address of the vCenter Server Appliance -
Username
is the username of the vCenter Server Appliance -
Password
is the password of the vCenter Server Appliance -
vcenterServerThumbprint
is the vCenter Server Appliance SHA1 Thumbprint
Once the maxView vSphere plugin is registered, the maxView icon is displayed in shortcut of vCenter Server Appliance (https://VCSA_IP/ui/app/shortcuts).
-
- Navigate to
- Click on the maxView icon to list
the ESXi systems added.Note: Initially, none of the system are added.
- Click on Add system to add the ESXi systems.
- Add the firewall entry by using
URL: https://VCSA_IP: 5480. Click on the firewall and add the entry.Note: Replace VCSA_IP with the user installed vCenter Server Appliance IP address.Note: The configuration or events are not delivered, if the firewall is not added.