4.5 Revealing More Device Information
Reveal more information about disk drive, array, and logical drive usage in the storage space (including maxCache Devices) with the Resources view on the Storage Dashboard.
To reveal disk drive usage by logical drive (and vice-versa), select a controller in the Enterprise View, then open the Resources tab on the Storage Dashboard. The following figure shows that clicking on a logical drive displays its member disk drives and spares; similarly, clicking on a physical disk displays which array (if any) it belongs to. In the following figure, the disk in Slot 1 and Slot 2 belongs to Array A.