6.7 Controller Sanitize Lock Freeze/Anti-Freeze
The Sanitize Lock Freeze/Anti-Freeze feature provides the controller level of sanitize lock, which helps prevent accidental erasing of data on the disk after initiating a sanitize command. To accomplish this, you have the option of applying a controller-wide Sanitize Lock Freeze/Anti-Freeze policy. The freeze and anti-freeze commands will be used to block and unblock the sanitize commands that would erase data on the disk.
The sanitize lock feature has three options:
Freeze: Prevents any sanitize erase operations to be performed
Anti-Freeze: Locks the freeze command and enables any sanitize erase operation to be performed
None: Enables any sanitize erase operation to be performed
This is applicable only to SATA drives which support Sanitize Erase, Freeze, and Anti-Freeze.
To set the Sanitize Lock:
- In the Enterprise View, select a controller.
- On the ribbon, in the Controller group, click Set Properties.
The Set Properties window opens. - Click the Data Protection tab.
- From the Sanitize Lock drop-down list, select one of the three following options: None (default), Freeze, or Anti-Freeze.
Note:If the Sanitize Lock is set to any value other than None, the following warning message will be displayed in the menu header:
Changing the Sanitize Lock will require a reboot to apply the new state to the controller, and require all physical devices to be power cycled or hot-plugged for the lock state to be applied to the physical devices. - Click OK.