8.1 maxCache Limitations
- maxCache is not supported on all Adaptec Smart Storage Controllers. For more information, see PMC-2153191 maxView Storage Manager and ARCCONF Command Line Utility Readme.
- If the maxCache controller has a green backup module, the super capacitor must be fully charged.
- Following are the limitations on maxCache device:
- It must be created with SSDs
- It must have logical block size of 512 bytes
Minimum maxCache device capacity is 16 GB
Maximum aggregate maxCache device sizes can be ~1.7TB for 64KB cache line size, ~6.8TB for 256KB cache line size.
Following are the limitations on the data logical device for which the maxCache device to be assigned:
- It must have the capacity at least as large as the maxCache device
- It must have logical block size of 512 bytes
Maximum data logical device size can be 256TB for the maxCache created with 64KB cache line size, 1024TB for the maxCache created with 256KB cache line size
For assigning maxCache to a SSD data logical device, SSD I/O bypass property should be disabled on the corresponding SSD data array
- The following operations are not available when maxCache is
enabled:
- Expand Array/Logical Device
- Move Logical Device
- Replace Array Drives
- Split Mirror
- Heal Array
- Migrate Array