14.6 Sending Events to the Windows Action Center
maxView is capable of sending events received from the local and managed system(s) to the Windows Action Center in the form of Toast notification. It is supported in a few latest versions of Windows Operating System.
Perform the following steps to change the Windows toast notification level on a
system:
- Select the Enterprise view node.
- On the ribbon, in the System
group, click System Settings.

The System Settings window opens for that system. The Windows Toast Notification Level setting appears under General tab.

- To change the Windows Toast Notification Level, click on the dropdown to select
from the following list of events to be sent to the Windows Activation
Center:
- None
- Error
- Error, Warning
- Error, Warning, Information
- Click OK to save the changes.