18.5 Deleting Host from maxView Plugin for VMware vSphere 8 or VMware vSphere 9 HTML Client

maxView plugin provides the delete system feature to delete one or more ESXi systems from the host list.
Note: Delete feature is only applicable when maxView plugin manages at least one ESXi system.
Perform the following steps to delete the ESXi systems:
  1. In the Monitoring section on the vSphere client's shortcut page screen, click maxView icon, The Host information screen appears.
  2. Click Delete System icon to delete the ESXi host.

    The Delete System dialog box appears.

  3. Select the ESXi host to be deleted.

  4. Click Delete.

    The status dialog box appears displaying the success or failure status message.

  5. Click OK.
  6. Click Global Refresh icon to remove the deleted system from the list.