6.7.1 Sanitize Lock Property in Controller Node Properties Tab
The properties of the Sanitize Lock feature are displayed in the controller node properties tab as shown in the following screen capture.
The Sanitize Lock property will display the current setting in which the controller is operating.
When the Sanitize Lock property is changed in the Set Properties dialog, the pending Sanitize Lock property will show the changed value.
When the machine is rebooted, the pending Sanitize Lock value will be "Not Applicable", and the Sanitize Lock value will be set to the previous pending Sanitize Lock value.