Jump to main content
30.4.1.9 Synchronous Host Reception Setup
Initialize the SPxBRGH:SPxBRGL
register pair and set or clear the BRG16 bit, as required, to achieve the desired baud rate.
Select the receive input pin by writing
the appropriate values to the RxyPPS and RXxPPS registers. Both selections may enable
the same pin.
Select the clock output pin by writing
the appropriate values to the RxyPPS and TXxPPS registers. Both selections may enable
the same pin.
Clear the ANSEL bit for the RXx pin (if applicable).
Enable the synchronous host serial port by setting the SYNC , SPEN and CSRC bits.
Ensure that the CREN and SREN bits are cleared.
If interrupts are desired, set the RCxIE bit of the PIEx
register and the GIE and PEIE bits of the INTCON register.
If 9-bit reception is desired, set the RX9
bit.
Start reception by setting the SREN bit, or for continuous
reception set the CREN bit.
The RCxIF Interrupt Flag bit will be set when reception of a
character is complete. An interrupt will be generated if the RCxIE enable bit was
set.
Read the RCxSTA register to get the ninth bit (if enabled) and determine
if any error occurred during reception.
Read the 8-bit received data by reading the RCxREG
register.
If an overrun error occurs, clear the error by either clearing
the CREN bit or by clearing the SPEN bit which resets the EUSART.
Figure 30-11. Synchronous Reception (Host Mode,
SREN)
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.