5.5 Revision 5
Revision 5 is the initially released revision. Figure 5-1 shows a top-down image of this revision alongside its assembly drawing.
There is a Kyocera Corporation ST3215SB32768C0HPWBB 7 pF crystal mounted on the 32.768 kHz crystal footprint on revision 5 of PIC16F18446 Curiosity Nano.
This revision has a different power supply circuit than the one described in Figure 3-4 3-5, in particular with regards to power protection used. Refer to Figure 5-2 instead.
Revision 5 does not have the Target Power strap, as described in Low Power Measurement. Instead, the current can be measured across the Power Supply strap, as described in Programming External Microcontrollers.
The holes along the edge connections are not staggered, as described in Using Pin Headers, and require soldering when mounting pin headers.