1 Harmony 3 Peripheral Library Application Examples for PIC32CX SG Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description |
|---|---|
| AC Sleepwalking | This example application shows how to use the AC Peripheral library to perform a single shot comparison in standby sleep mode periodically and wake up the device at the end of a successful comparison |
| ADC DMA Sleepwalking | This application shows how to configure the ADC in a sleepwalking operation, where the input voltage is measured at a fixed interval, and then the device is woken from sleep after conversion of 16 samples |
| ADC Window Sleepwalking | This application shows how to configure ADC in a sleepwalking operation, where input voltage is measured at a fixed interval, but device is not woken from sleep until the measured value is below a given threshold |
| Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification |
| DMAC CRC-32 Generation | This example application demonstrates how to use the DMAC peripheral to compute 32-bit Cyclic Redundancy Checksum (CRC) |
| DMAC Memory Transfer | This example application demonstrates how to use the DMAC peripheral to do a memory to memory transfer |
| DMAC USART Echo | This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes |
| DSU Compute CRC32 | This example application demonstrates how to use the DSU Peripheral library to compute 32-bit Cyclic Redundancy Checksum (CRC) |
| EIC Interrupt | This example application demonstrates how to generate interrupt using the EIC on switch press and indicate it through an LED |
| NVMCTRL Read Write | This example application demonstrates how to use the NVMCTRL to erase and program the internal Flash memory |
| PM Wakeup Using EIC | This application demonstrates entering the low power modes and exiting it using the EIC |
| PM Wakeup Using RTC | This example demonstrates entering the low power modes and exiting it using the RTC |
| PORT Polling | This example application demonstrate how to poll the switch input, and indicate the switch status using the LED |
| RTC Alarm Interrupt | This example shows how to use the RTC to configure the time and generate the alarm |
| RTC Periodic Interrupt | This example application shows how to use the RTC to generate periodic interrupts |
| SERCOM SPI Blocking | This example application demonstrates how to use the SERCOM SPI peripheral to transmit and receive a block of data in a blocking manner |
| SERCOM SPI Interrupt | This example application shows how to use SERCOM SPI PLIB with external loop back to write and then read back an array of data in interrupt mode |
| SERCOM SPI Ping Pong with DMA | This example demonstrates how to continuously transmit and receive data over a SPI interface using ping pong buffers with DMA |
| SERCOM USART Blocking | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer block of data in a blocking manner |
| SERCOM USART Interrupt | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer data in a non-blocking manner |
| SERCOM USART Ring Buffer | This example application demonstrates how to use the SERCOM peripheral in USART ring buffer mode to transfer data in a non-blocking manner |
| Systick Periodic Interrupt | This example shows how to use the SysTick to generate periodic interrupts |
| TC Timer Mode | This example shows how to use the TC module in timer mode to generate periodic interrupt |
| WDT Timeout | This example shows how to generate a Watchdog timer reset by emulating a deadlock |