6 Kit Specific Data
One of the Flash user pages in the EDBG is programmed with data specific to the SAM E54 Xplained Pro. The data can be read through the I2C interface connected to the EDBG from the target application. For detailed information, refer to the EDBG User Guide. All data is stored as little endian. The table below shows the memory map for the Flash user page.
| Name | Description | Size [bits] |
|---|---|---|
| MAC48 | Unique address assigned to the kit, value taken from the onboard AT24MAC402. | 48 |