40.5.6 Low-Pass Filter Mode
The Low-Pass Filter mode (MD =
‘b100
) acts
similarly to the Average mode in how it handles samples (accumulates samples until the
ADCNT value is greater than or equal to RPT, then
triggers a threshold comparison), but instead of a simple average, it performs a
low-pass filter operation on all of the samples, reducing the effect of high-frequency
noise on the total, then performs a threshold comparison on the results. In this mode,
the CRS
bits determine the cutoff frequency of the low-pass filter (as demonstrated by Digital
Filter/Average). Refer to the Computation
Operation section for a more detailed description of the mathematical
operation.For more information about Low-Pass Filter mode, refer to the
following Microchip application note, available in the corporate website (www.microchip.com):
- AN2749, “PIC18 12-bit ADCC in Low-Pass Filter Mode”