3.6.3.2 Debugging License Issues
(Ask a Question)- Double check the
LM_LICENSE_FILE
is printed correctly in the SmartHLS license error message:Error: There is a problem with your SmartHLS feature license. Your current environment variable is: LM_LICENSE_FILE=1702@server.domain.com Please modify your LM_LICENSE_FILE environment variable and restart SmartHLS.
Important: If you changed yourLM_LICENSE_FILE
environment variable then you will need to restart the SmartHLS IDE to detect the change. - Otherwise, on Windows run Start and launch the command prompt. In the command prompt, run the following command to debug issues checking out the “SmartHLS” feature:
C:\Microchip\Libero_SoC_v<version>\Designer\bin\lmutil.exe lmdiag SmartHLS
Where
<version>
is the Libero SoC release version.Make sure you can seeThis license can be checked out.
For example:----------------------------------------------------- License file: 1702@server.domain.com ----------------------------------------------------- "SmartHLS" v2022.08, vendor: actlmgrd, expiry: 14-aug-2041 License server: 10.241.70.175 floating license expires: 14-aug-2041 This license can be checked out
If not, you will need to update your
license.dat
file to include the SmartHLS feature line. - You can also check how many SmartHLS licenses are in use using the following command.
C:\Microchip\Libero_SoC_v<version>\Designer\bin\lmutil.exe lmstat -f SmartHLS
Where
<version>
is theLibero SoC release version.