19.4.4.4 Checking Cascaded Math Block Instance Adherence to the Separation Criteria
(Ask a Question)MSVT checks if all of the cascaded Math block instances adhere to the separation criteria. If there are any cascaded Math block instances that violate the separation criteria, then they are listed in the Input signals of the following Math block instances can be observed by failure of config switches in cascade chain
section of the report.
Design Example
The following is a chip planner snap shot of a design in which Top_sign21x18_mult_0
, Top_sign21x18_mult_1
and Top_sign21x18_mult_2
are three Math blocks. Top_sign21x18_mult_0
is adjacent to Top_sign21x18_mult_1
, whereas Top_sign21x18_mult_2
is separated by Top_sign21x18_mult_1
with one MATH
cluster.
MSVT Output Report
Because Top_sign21x18_mult_0
is adjacent to Top_sign21x18_mult_1
, MSVT fails and reports an error for these MACC
instances, as shown in the following. However, asTop_sign21x18_mult_2
is separated from Top_sign21x18_mult_1
by at least one MATH
cluster, it is not identified as an error by MSVT, as shown in following report section example.
Input signals of the following Math block instances can be observed by failure of the config switches in the cascade chain
-----------------------------------------------------------------------------------------------------------------------------------------
Input signals of the following Math block instances can be observed by failure of the config switches in the cascade chain: ================================================================================================================== Block1_rom_0/macc_rom_top/MACC_PA_BC_ROM_5/MACC_PHYS_0/INST_MACC_IP of block Block1_rom_0 can be observed by Math block instance Block0_0/block0_level_0/MACC_PA_8/MACC_PHYS_INST/INST_MACC_IP of block Block0_0
-----------------------------------------------------------------------------------------------------------------------------------------