8.2 Fold Instance
(Ask a Question)The expanded hierarchy of an instance can be folded or collapsed back into the parent instance.
Use one of the following three ways to fold/collapse the expanded instance back into the parent instance:
- Click the - button at the top left of the instance.
- Click to select the expanded instance, then right click and select Fold Instance in the menu.
- Click the Fold All Instance icon.