9.9.1.3 Region Assignments
(Ask a Question)When you right click an item in one of the tabs in the Main Object Browser, you can choose from available options, which can include placing an item to a location, unplacing an item from a location, locking the placement, and assigning a region.
Multiple items can be selected and assigned to the same region at the same time. You can also select a region assignment by right clicking an item and choosing Region Assign. The dialog box opens as shown in the following figure. This option is not available for objects in the Region tab.