8.1.4.6 Log Window
(Ask a Question)The Log window displays the following:
- Informational messages such as the location and name of the files used to display the view.
- Any syntax errors in the HDL file if the HDL file is opened with the Open File Location option (right click design object > Open File Location).
Important: The Log window displays by default
when the Netlist Viewer opens. Hiding the Log
window will leave more display area for the Canvas view. To get a larger display area for the
Canvas view, hide the Log window ( and uncheck (Show Log).