3.6.8.2.1 Step 1 - Setup Required Board Connections
(Ask a Question)Important: Micro USB sockets on the Icicle board are very fragile and can easily break. Be careful when plugging/unplugging the micro USB cables. Also micro USB cables can occasionally fail, so try another cable.
The following cables must be connected to the Icicle Kit for use with SmartHLS™:
- Power cable (connects to
12V Power Supply Input
). - Micro USB for transferring the image to the board (one end connects to
USB OTG
, while the other end connects to the host PC that will transfer the image).- This cable is used to expose the internal eMMC memory as a USB storage
- Required only if the Linux image needs to be updated
- Micro USB for serial communication to the board (one end connects to
USB - UART Terminal
, while the other end connects to the host PC).- This cable is used to open a serial communication terminal between the Linux system on the board and the host PC.
- Required only if serial communication is required (for Linux image transfer or determining the board’s network IP address).
- FlashPro6 programmer, embedded or external, connected to the host PC.
- For an embedded programmer, connect a micro USB cable to
USB Embedded Programming Connector
, and make sure that jumpers J9 and J24 are closed. - For an external programmer, connect it to
JTAG Programming Header
, and make sure that jumpers J9 is open.
- For an embedded programmer, connect a micro USB cable to
- Ethernet cable, one end connected to
GEM1
, and the other end connected either directly to the PC, or to the same network as the host PC (for example, the same router). Tip: On Dell laptops to enable both Ethernet and WiFi at the same time you may have to modify your bios settings.