6.5.1 Importing a Block
(Ask a Question)To import a block:
- From the File menu, choose Import > Blocks.
- Browse to the directory that contains the <design_block_name>.cxz file, and then select the file.
- Click Open.
The <design_block_name> file is imported into the top_level
project. Version control is not supported for imported blocks. If you import the same block twice, the new block overwrites the existing block.
Files are imported under the <design>\component\work\<design_block_name> folder. See the Block reports in the directory.