15.1.13 FlashPro Express Reference
(Ask a Question)Use this chapter as a reference for the FlashPro Express user interface.
15.1.13.1 FlashPro Express Start Page
(Ask a Question)The FlashPro Express Start page is the first page that appears when the tool starts. This page provides the interface for loading a project into the tool by either navigating to the project location or clicking a recently opened project.
15.1.13.2 FlashPro Express Project Menu
(Ask a Question)The following table lists the FlashPro express project menu details.
Command | Function |
---|---|
New Job Project | New job project folder with programming job name will be created at the specified location. |
Open Job Project | Loads a job project into the tool by reading the information in the user-specified |
Close Job Project | Closes the current job project. |
Save Job Project | Saves the current job project. |
Set Log File | Sets the location of the Log file to your specified location. |
Export Log File | Exports the Log file to your specified location. |
Preferences | Allows you to select FlashPro Express mode. |
Execute Script | Runs your specified Tcl script. |
Export Script File | Exports all commands run in this session to your specified path as a Tcl script. |
Exit | Exits FlashPro Express. |
15.1.13.3 FlashPro Express Edit Menu
(Ask a Question)Command | Function |
---|---|
Clear Log Window | Clears the Log window. |
15.1.13.4 FlashPro Express View Menu
(Ask a Question)Command | Function |
---|---|
Log Window | Shows or hides the Log window. |
15.1.13.5 FlashPro Express Tools Menu
(Ask a Question)The following table lists the FlashPro express tools menu details.
Command | Function |
---|---|
Programming Connectivity and Interface | The Programming Connectivity and Interface window displays the physical chain from TDI to TDO or SPI Target configuration. |
Programmer Settings | Opens the Programmer Settings dialog box in which you can set options for supported Microchip programmers. |
Disable Core Check During Scan and Check Chain | Disables core checking during scan and check chain operations. |
15.1.13.6 FlashPro Express Help Menu
(Ask a Question)Command | Function |
---|---|
Help Topics | Opens the help. |
Microchip Technical Support | Opens the Microchip technical support site. |
Microchip Web Site |
Opens the Microchip Website in your default browser. |
User Guide | Opens the FlashPro Express User Guide. |
Check for Software Updates | Checks for software updates if you are connected to the Internet. |
About FlashPro Express | Lists the FlashPro Express release information. |
15.1.13.7 FlashPro Express Log Window and Status Bar
(Ask a Question)The following sections describe the FlashPro Express Log window and status bar.
15.1.13.7.1 FlashPro Express Log Window
(Ask a Question)The FlashPro Express Log window shows status messages for user activity.
- Click the appropriate tab (Messages, Errors, Warning, and Info) to filter messages by type.
- Use the right-click menu to copy text, clear the log, and scroll the log.
- Use the def variable LOG_WINDOW_BUFFER_SIZE to set the buffer size.
- Use the View menu to show or hide the Log window.
15.1.13.7.2 FlashPro Express Status Bar
(Ask a Question)The Status Bar at the bottom shows the status of the load project action.