9.6.4 Making I/O Assignments
(Ask a Question)To make I/O assignment for the Memory Interface instance in the design:
- Select the Memory Interface type from the drop-down menu.
- From the Ports tab in the Design Tree View, drag the Memory Interface instance and let the mouse hover over one of the Edge_Anchor locations available for the Memory Interface type. A tooltip reports whether it is a legal or illegal location for the Interface instance.
- Drop the Interface instance into a legal Edge_Anchor location.
-
Check that no DRC error messages are reported in the Log window
and the I/O assignments are accepted (see the following figure). The Lock icon in the
Ports tab indicates that the I/O assignment is accepted and locked.
Figure 9-9. Memory Interface Assignments Accepted
Note: DRC rules are enforced. Drag-and-drop I/O placement that violates the DRC rules
are reported in the Log window. For Memory Interface, the DRC checks the Data
Width and the Data Rate compliance*. If the specific location cannot accommodate
the Data Width or the Data Rate of the Memory interface, no I/O assignment is
made. An error is reported in the Log Window with a message that explains why the
assignment is not accepted. In the following figure, the DRC error message reports
that the ddr3 instance requires 64 ports, but the SOUTH_SE location can
accommodate only 58 pins.
Note: *Data Rate compliance will be enforced in a later release.