Informational messages such as the
location and name of the files used to display the view.
Any syntax errors in the HDL file if the
HDL file is opened with the Open File Location option (right click
design object > Open File Location).
Important: The Log window displays by default
when the Netlist Viewer opens. Hiding the Log
window will leave more display area for the Canvas view. To get a larger display area for the
Canvas view, hide the Log window (Netlist Viewer > Windows and uncheck (Show Log).Figure 8-17. Log Window