15.1.1 Overview
(Ask a Question)This section provides an overview of FlashPro Express.
15.1.1.1 FlashPro Hardware Programmers
(Ask a Question)- FlashPro3/X
- FlashPro4
- FlashPro5
- FlashPro6
For more information, visit the Microchip Website .
15.1.1.2 Secure Job Programming
(Ask a Question)Job programming is the concept of using a single file to program a Microchip device or chain of Microchip devices using encrypted bitstreams.
The single job file contains all of the information necessary to setup FlashPro Express as well as the encrypted bitstream images for the devices in the job. After a job file is created, it can be passed securely to production programming houses or contract engineering facilities to load the Microchip images during manufacturing. Job projects can be exported from Libero and imported into stand-alone FlashPro Express, providing a clean delineation between design flow and production programming.
15.1.1.3 Migrating FlashPro Projects to FlashPro Express
(Ask a Question)Existing FlashPro projects (*.pro
) files are called Job Project files in
FlashPro Express. These Job Projects can be opened with FlashPro Express to take
advantage of Linux programming support and the simplified tool targeted for operators in
a production floor environment.
To convert the project to a chain project:
- Open the FlashPro project
(
*.pro
) in FlashPro. - Locate the loaded STAPL file by one of two
methods:
The log prints STAPL file ‘<stapl_path>’ has been loaded successfully. <stapl_path> is the location of the STAPL file loaded.
Figure 15-1. Sample Log Message

- Switch the project to chain mode using one of the
two methods:
- Press the chain button from the toolbar:
- From the Tools menu, select Mode > Chain Programming.
- Press the chain button from the toolbar:
- Load the STAPL file in chain mode by adding a
Microchip device in the chain.
- From the File menu, select Configuration > Add Microchip Devices from Files.
- Browse to the location of the STAPL file and click Open.
- To save the project, from the File menu, select Save Project.
You can now open the project using FlashPro Express.
When moving FlashPro project (*.pro
) files to another machine, Microchip
recommends that you archive the entire project folder, copy it to the new machine,
extract it locally, and then load the job project within FlashPro Express. FlashPro
Express opens a job project only when a programmer is connected to the machine, at least
one Microchip device has programmed enabled, and all enabled Microchip devices have a
bitstream file loaded.