11.9 A - Limitations
(Ask a Question)This appendix lists Chip Planner limitations.
11.9.1 I/O Register Support
(Ask a Question)Every I/O has several embedded registers that you can use for faster clock-to-out timing, and to meet external hold and setup timing requirements. This feature uses input, output, or enable registers available in the I/O block.
However, a register (if combined with an I/O register) is not shown in the Logical view as a separate element and is shown as part of a port.

11.9.2 Internal Elements of External IP Macros Displayed in a Single Connection
(Ask a Question)Some external IP, such as SerDes and FDDR, spans across multiple clusters and has its own dedicated ports. However, the net connected to these macro I/Os are shown to be connected from a single location. The following figure is an example of a SerDes macro that shows all the associated nets connected to a single macro.

11.9.2.1 Cross-Probing into SmartTime Not Supported
(Ask a Question)Cross-probing from the Chip View /Netlist View into SmartTime is not supported. Cross-probing is supported for SmartTime to Chip View and Netlist View, but not from Chip View or Netlist View to SmartTime.