16.1.5 Special

16.1.5.1 FCEND_BUFF

Buffer, driven by the FCO pin of the last macro in the Carry-Chain.
Figure 16-62. FCEND_BUFF
Table 16-123. FCEND_BUFF I/O
InputOutput
AY
Table 16-124. FCEND_BUFF Truth Table
AY
00
11

16.1.5.2 FCINIT_BUFF

Buffer, used to initialize the FCI pin of the first macro in the Carry-Chain.
Figure 16-63. FCINIT_BUFF
Table 16-125. FCINIT_BUFF I/O
InputOutput
AY
Table 16-126. FCINIT_BUFF Truth Table
AY
00
11

16.1.5.3 PF_SPI

The PF_SPI macro allows your design access to the dedicated System Controller SPI port, when SPI-​Initiator mode is enabled, by tying both SC_SPI_EN and IO_CFG_INTF to high.
Figure 16-64. PF_SPI
Table 16-127. Ports and Descriptions
PortDirectionPolarityDescription
D_IOutputThis port is connected to the SPI DI pin.
FAB_SPI_OWNEROutputHighIndicator to the Fabric SPI-​Initiator if the SPI Port is available.
CLK_OEInputHighEnables the SPI CLK output.
CLK_OInputThis port drives the SPI Clock pin. CLK_OE must be HIGH to drive.
D_OEInputHighEnables the Data output.
D_OInputThis port drives the SPI DO pin. D_OE must be HIGH to drive.
SS_OEInputHighEnables the Target Select output.
SS_OInputHighThis port drives the SPI Target Select (SS) pin. SS_OE must be HIGH to drive.
CLKOutputSPI Clock output pin.
DIInputSPI Serial Data input pin.
DOOutputSPI Serial Data output pin.
SSOutputHighSPI Target Select output pin.
IFACEInputHighThis port is mapped to the IO_CFG_INTF pin. This pin must be tied to high together with the SC_SPI_EN pin to enable SPI port for the fabric macro to work.
FLASHInputHighThis port is mapped to the SC_SPI_EN pin. This pin must be tied to high together with the IO_CFG_INTF pin to enable the SPI port for fabric macro to work.

16.1.5.4 SC_STATUS

In the SC_STATUS macro, the SUSPEND_EN signal indicates that the device is in Avionics mode, meaning device initialization is complete and all hardware defaults are set.
Important: This macro does not support simulation. To simulate the System Controller Suspend mode, add the following pseudo-code to the simulation testbench:
  • At simulation time t = 0, set SUSPEND_EN = 0, and ACTIVE = 1.
  • At 0.625 µs after the later assertion of DEVICE_INIT_DONE = 1 or AUTOCALIB_DONE = 1, set SUSPEND_EN = 1, and ACTIVE = 0 to indicate that the System Controller has entered Suspend mode.
Figure 16-65. SC_STATUS
Table 16-128. SC_STATUS I/O
Value of SUSPEND_ENDescription
0The device is not in Avionics mode.
1The device is in Avionics mode.
Table 16-129. Ports and Descriptions
PortWidthDirectionDescription
SUSPEND_EN1OutputAsserted when the System Controller is in Suspend mode.
ACTIVE1OutputAsserted when the System Controller is in Active mode.

The System Controller Suspend mode works as follows:

  • When JTAG_TRST_B is asserted low:
    • SUSPEND_EN is asserted high.
    • ACTIVE is asserted low.
  • When JTAG_TRST_B is asserted high:
    • SUSPEND_EN is asserted low.
    • ACTIVE is asserted high when the System Controller is actively performing a function.

The following table shows the state after the System Controller has finished its operations and entered Suspend mode, not just when the Suspend mode setting is enabled.

Table 16-130. SC_STATUS Expected Results
PortDirectionSuspend Mode EnabledSuspend Mode Disabled
SUSPEND_ENOUTPUT10
ACTIVEOUTPUT01, when the System Controller is actively performing a function.

Before performing operations that require the System Controller, like programming or debugging, ensure the device is not in Suspend mode.

Important: Enabling Suspend mode in Libero does not immediately restrict the System Controller. The restriction takes effect only after the controller completes initialization and enters Suspend mode.

16.1.5.5 OSC_RC160MHZ

The OSC_RC160MHZ oscillator is an RC oscillator that provides a free-running clock of 160 MHz at CLK when OSC_160MHZ_ON is tied HIGH.

16.1.5.6 OSC_RC2MHZ

The OSC_RC2MHZ oscillator is an RC oscillator that provides a free-running clock of 2 MHz at CLK when OSC_2MHZ_ON is tied HIGH.

16.1.5.7 LIVE_PROBE_A

This is one of the specialized probes. SmartDebug uses the dedicated and specialized probe points built in the FPGA fabric, which significantly accelerates and simplifies the debug process.

16.1.5.8 INIT

This macro does do not have any inputs. It has the following output ports, which are asserted after the specified time that is passed as parameters.
  • FABRIC_POR_N: De-asserted when the fabric is operational.
  • PCIE_INIT_DONE: Used by fabric logic to hold PCIe-related fabric logic in reset until the PCIe controller is initialized. PCIE_INIT_DONE is asserted after initializing the PCIe lane instances placed in the PCIe quad. If only XCVR lanes are placed in the PCIe quad, only XCVR_INIT_DONE is asserted.
  • RFU[0]: Asserted when the XCVR block is initialized.
  • RFU[1]: Asserted when μSRAM is initialized from sNVM.
  • RFU[2]: Asserted when μSRAM is initialized from µPROM.
  • RFU[3]: Asserted when μSRAM is initialized from SPI.
  • RFU[4]: Asserted when SRAM is initialized from sNVM.
  • RFU[5]: Asserted when SRAM is initialized from µPROM.
  • RFU[6]: Asserted when SRAM is initialized from SPI.
  • RFU[7]: Asserted when auto calibration is done.
  • SRAM_INIT_DONE: Asserted when the LSRAM blocks are initialized.
  • USRAM_INIT_DONE: Asserted when the µSRAM blocks are initialized.
  • GPIO_ACTIVE: This signal can be used by user logic to determine if the calibration completes for each I/O banks. # denotes the bank number (0,1, 7, 8, and 9).
  • HSIO_ACTIVE: This signal can be used to monitor if there is VDDI power loss on specific I/O banks. This is an output signal from the INIT_MONITOR IP if any of the corresponding bank is selected. # denotes the bank number (0,1, 7, 8, and 9).

16.1.5.9 LANECTRL

The lane controller handles the complex operations necessary for the high-speed interfaces, such as DDR memory and CDR interfaces. To bridge the lane clock to the high-speed I/O clock, the lane controller is used to control an I/O FIFO in each IOD. The I/O FIFO interfaces with DDR memory by using the Data Q Strobe (DQS) on the lane clock. The lane controller can also delay the lane clock using a Process, Voltage, and Temperature (PVT)-calculated delay code from the DLL to provide a 90° shift. Certain I/O interfaces require a lane controller to handle the clock-domain that results with higher gear ratios. The lane controller also provides the functionality for the IOD CDR. Using the four phases from the CCC PLL, the lane controller creates eight phases and selects the proper phase for the current input condition with the input data.

16.1.5.10 LANECTRL_BYPASS

This macro puts the LANECTRL in bypass mode. It has three ports A, RESET and CLK_OUT_R.

16.1.5.11 PFSOC_SCSM

The PFSOC_SCSM macro allows a PolarFire SoC device, configured with the System Controller Suspend Mode (SCSM) enabled, to support MSS reboots during normal device operation. Without this macro, the System Controller:

  • Will remain in suspend mode during normal operation after the initial power-up device initialization and MSS boot completion.
  • Will not service subsequent MSS boot requests, even if you reset the MSS.

You must connect the REBOOT_REQUESTED_M2F output of the MSS component to the SC_WAKE input pin of the PFSOC_SCSM macro. Other connections are not permitted.

Important: To enable the REBOOT_REQUESTED_M2F port in the MSS configurator, check the Expose Feedback ports to Fabric option under the Misc tab.

With this connection added to your FPGA fabric design, whenever the MSS REBOOT_REQUESTED_M2F output is asserted, the System Controller exits SCSM and processes the pending MSS reboot request. Once the MSS boots, the REBOOT_REQUESTED_M2F output will deassert and the System Controller returns to the suspend mode. The System Controller status can be monitored via the SC_STATUS macro.

Important: The PFSOC_SCSM macro only supports the PolarFire SoC (production device) family. PolarFire SoC Engineering Silicon (ES) devices are not supported.
Figure 16-66. PFSOC_SCSM Macro

Design Rule Checks

Following are the Design Rule Checks (DRCs) for the PFSOC_SCSM macro.

  • Check that the driver is only MSS REBOOT_REQUESTED_M2F, otherwise the PFSOC_SCSM macro will error out and stop the flow with the following message:
    The PFSOC_SCSM primitive macro only supports being driven by the MSS component’s REBOOT_REQUESTED_M2F output. Other drivers are not supported. See the PolarFire SoC Macro Library Guide for more information.
  • If Suspend is not enabled, and the PFSOC_SCSM is instantiated, a warning is issued in the Export Design Initialization Data and Memory Report file.
    The PFSOC_SCSM macro is instantiated in the design, but System Controller Suspend Mode is not enabled. This macro is intended for use with System Controller Suspend Mode. See the PolarFire SoC Macro Library Guide for more information.
  • If Suspend is enabled, and the MSS is used, but the PFSOC_SCSM macro is not instantiated, a warning is issued in the Export Design Initialization Data and Memory Report file.
    The PFSOC_SCSM macro is not instantiated even though System Controller Suspend Mode is enabled and the MSS component is instantiated. The system controller will not be available to process MSS reboot requests during operation. See the PolarFire SoC Macro Library Guide for more information.
  • The PFSOC_SCSM macro is visible only for the PolarFire SoC designs. This macro is required for the PolarFire SoC designs using the MSS component and for enabling System Controller Suspend Mode (SCSM). When not used in the PolarFire SoC designs, Libero ties the input to the System Controller to a static 1.
  • If an ES device or a PolarFire family is selected, the PFSOC_SCSM macro will error out and stop the flow in compile with the following error message, as only production PolarFire SoC devices are supported.
    CMPPF_026: This design has one or more instances of the PFSOC_SCSM macro which is not supported for the device in use. Before compiling, this macro(s) must be removed from the design.
  • For RT PolarFire SoC devices:
    Error: The PFSOC_SCSM pin cannot be static. Refer to the PolarFire SoC Macro Library Guide for more information."