21.13.1.76 unset_live_probe
(Ask a Question)Description
This Tcl command discontinues the debug function and clears both live probe channels (Channel A and Channel B). An all zeros value is shown for both channels in the oscilloscope.
For RTG4, only one probe channel (Probe Read Data Pin) is available.
unset_live_probe [-deviceName "device name"] \
[-probeA "TRUE | FALSE"] \
[-probeB "TRUE | FALSE"]'Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Parameter is optional if only one device is available in the current configuration. |
probeA | boolean | Specify 1 or TRUE for unset live probe on Channel A, otherwise specify 0 or FALSE. |
probeB | boolean | Specify 1 or TRUE for unset live probe on Channel B, otherwise specify 0 or FALSE. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Cannot unset live probes: Mention the name of the channel to unset. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'unset_live_probe [-deviceName "device name"] [-probeA "TRUE | FALSE"] [-probeB "TRUE | FALSE"]'. |
None | probeA: Invalid argument value: (expecting TRUE, 1, true, FALSE, 0 or false). |
None | probeB: Invalid argument value: (expecting TRUE, 1, true, FALSE, 0 or false). |
None | Parameter 'deviceName' has illegal value. |
Supported Families
| PolarFire |
| PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
The following example unsets both live probe channels (Channel A and Channel B) from the device sf2:
unset_live_probes -probeA 1 -probeB 1 [-deviceName {sf2}]See Also
set_live_probe