21.6.9 GENERATEPROGRAMMINGFILE

Description

"GENERATEPROGRAMMINGFILE" is a command tool used in the configure_tool and run_tool commands. The configure_tool -name {GENERATEPROGRAMMINGFILE} Tcl command configures tool options. The run_tool -name {GENERATEPROGRAMMINGFILE} Tcl command runs the specified tool with the options specified in configure_tool.

Important: The tools have the new Tcl parameters sanitize_snvm (PolarFire, RT PolarFire, and PolarFire SoC) and sanitize_envm (SmartFusion 2, IGLOO 2, and PolarFire SoC) available from Libero v12.6.

The command usage for the PolarFire is the following:

configure_tool -name {GENERATEPROGRAMMINGFILE} \
               -params {program_fabric: true | false } \
               -params {program_security: true | false } \
               -params {program_snvm: true | false} \
               -params {sanitize_snvm: true | false}
run_tool -name {GENERATEPROGRAMMINGFILE}

The command usage for the RTG4 is the following:

configure_tool -name {GENERATEPROGRAMMINGFILE} \
               -params {program_fabric: true | false } \
               -params {program_security: true | false } \
               -params {program_mode:selected_features} \
               -params {program_envm: true | false} \
               -params {sanitize_envm: true | false} 
run_tool -name {GENERATEPROGRAMMINGFILE}

The command usage for the SmartFusion 2, IGLOO 2 is the following:

configure_tool -name {GENERATEPROGRAMMINGFILE} \
               -params {program_fabric: true | false } \
               -params {program_security: true | false } \
               -params {program_snvm: true | false} \
               -params {sanitize_snvm: true | false} 
run_tool -name {GENERATEPROGRAMMINGFILE}

The command usage for the PolarFire SoC is the following:

configure_tool -name {GENERATEPROGRAMMINGFILE} \
               -params {program_fabric_snvm: true | false} \
               -params {program_security: true | false} \
               -params {program_envm: true | false} \
               -params {sanitize_envm: true | false} \
               -params {sanitize_snvm: true | false}
run_tool -name {GENERATEPROGRAMMINGFILE}

Arguments

The following table list the "GENERATEPROGRAMMINGFILE" arguments for PolarFire.

ParameterTypeDescription
program_fabricbooleanInclude fabric component in the programming bitstream. The acceptable values are: true, false.
program_securitybooleanInclude custom security component in the programming bitstream ("true" only if custom security was defined). The acceptable values are: true, false.
program_snvmbooleanInclude sNVM component in the programming bitstream ("true" only if sNVM available in the design). The acceptable values are: true, false.
sanitize_snvmbooleanEnable eNVM sanitization.

The following table list the "GENERATEPROGRAMMINGFILE" arguments for RTG4.

ParameterTypeDescription
program_fabricbooleanInclude fabric component in the programming bitstream. The acceptable values are: true, false.
program_modestringThe possible value is "selected_features."
program_securitybooleanInclude custom security component in the programming bitstream ("true" only if custom security was defined). The acceptable values are: true, false.
program_envmbooleanInclude eNVM component in the programming bitstream ("true" only if eNVM available in the design). The acceptable values are: true, false.
sanitize_envmbooleanEnable eNVM sanitization.

The following table list the "GENERATEPROGRAMMINGFILE" arguments for SmartFusion 2, IGLOO 2.

ParameterTypeDescription
program_fabricbooleanInclude fabric component in the programming bitstream. The acceptable values are: true, false.
program_securitybooleanInclude custom security component in the programming bitstream ("true" only if custom security was defined). The acceptable values are: true, false.
program_envmbooleanInclude eNVM component in the programming bitstream ("true" only if eNVM available in the design). The acceptable values are: true, false.
sanitize_snvmbooleanEnable sNVM sanitization.

The following table list the "GENERATEPROGRAMMINGFILE" arguments for PolarFire SoC.

ParameterTypeDescription
program_fabric_snvmbooleanInclude Fabric/sNVM component in the programming bitstream. The acceptable values are: true, false.
program_securitybooleanInclude custom security component in the programming bitstream ("true" only if custom security was defined). The acceptable values are: true, false.
program_envmbooleanInclude eNVM component in the programming bitstream ("true" only if eNVM available in the design). The acceptable values are: true, false.
sanitize_envmbooleanEnable eNVM sanitization.
sanitize_snvmbooleanEnable sNVM sanitization.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneYou must select at least one component to program.
NoneParameter program_snvm does not exist.
NoneParameter program_envm does not exist.
NoneFabric/sNVM is not selected for programming; sNVM sanitization is not available.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

Configure "GENERATEPROGRAMMINGFILE" for PolarFire device:

configure_tool -name {GENERATEPROGRAMMINGFILE} \
               -params {program_fabric:false} \
               -params {program_security:true} \
               -params {program_snvm:true} 

See Also

  • GENERATEPROGRAMMINGDATA