16.3.1 All Macros

16.3.1.1 AND2

2-Input AND.
Figure 16-168. AND2
Table 16-361. AND2 I/O
InputsOutput
A, BY
Table 16-362. AND2 Truth Table
ABY
X00
0X0
111

16.3.1.2 AND3

3-Input AND.
Figure 16-169. AND3
Table 16-363. AND3 I/O
InputOutput
A, B, CY
Table 16-364. AND3 Truth Table
ABCY
XX00
X0X0
0XX0
1111

16.3.1.3 AND4

4-Input AND.
Figure 16-170. AND4
Table 16-365. AND4 I/O
InputOutput
A, B, C, DY
Table 16-366. AND4 Truth Table
ABCDY
XXX00
XX0X0
X0XX0
0XXX0
11111

16.3.1.4 CFG1/2/3/4 and Look-Up Tables (LUTs)

CFG1, CFG2, CFG3, and CFG4 are post-layout LUTs that implement any 1-input, 2-input, 3-input, and 4-input combinational logic functions respectively. Each of the CFG1/2/3/4 macros has an INIT string parameter that determines the logic functions of the macro. The output Y is dependent on the INIT string parameter and the values of the inputs.

16.3.1.5 CFG2

Post-layout macro implements any 2-input combinational logic function. Output Y is dependent on the INIT string parameter and the value of A and B. The INIT string parameter is 4 bits wide.
Figure 16-171. CFG2
Table 16-367. CFG2 I/O
InputOutput
A,BY = f (INIT, A, B)
Table 16-368. CFG2 INIT String Interpretation
BAY
00INIT[0]
01INIT[1]
10INIT[2]
11INIT[3]

16.3.1.6 CFG3

Post-layout macro used to implement any 3-input combinational logic function. Output Y is dependent on the INIT string parameter and the value of A, B, and C. The INIT string parameter is 8 bits wide.
Figure 16-172. CFG3
Table 16-369. CFG3 I/O
InputOutput
A, B, CY = f (INIT, A,B, C)
Table 16-370. CFG3 INIT String Interpretation
CBAY
000INIT[0]
001INIT[1]
010INIT[2]
011INIT[3]
100INIT[4]
101INIT[5]
110INIT[6]
111INIT[7]

16.3.1.7 CFG4

Post-layout macro used to implement any 4-input combinational logic function. Output Y is dependent on the INIT string parameter and the value of A, B, C, and D. The INIT string parameter is 16 bits wide.
Figure 16-173. CFG4
Table 16-371. CFG4 I/O
InputOutput
A, B, C, DY = f (INIT, A,B, C, D)
Table 16-372. CFG4 Truth Table
DCBAY
0000INIT[0]
0001INIT[1]
0010INIT[2]
0011INIT[3]
0100INIT[4]
0101INIT[5]
0110INIT[6]
0111INIT[7]
1000INIT[8]
1001INIT[9]
1010INIT[10]
1011INIT[11]
1100INIT[12]
1101INIT[13]
1110INIT[14]
1111INIT[15]

16.3.1.8 BUFF

Buffer.

Figure 16-174. BUFF
Table 16-373. BUFF
InputOutput
AY
Table 16-374. Truth Table
AY
00
11

16.3.1.9 BUFD

Buffer.
Note: The compile optimization does not remove this macro.
Figure 16-175. BUFD
Table 16-375. BUFD I/O
InputOutput
AY
Table 16-376. BUFD Truth Table
AY
00
11

16.3.1.10 BUFD_DELAY

Buffer. The cell delay of BUFD_DELAY is about 0.4 ns at Military operating conditions. Its delay is longer than that of BUFD.
Note: Compile optimization will not remove this macro.
Figure 16-176. BUFD_DELAY
Table 16-377. BUFD_DELAY
InputOutput
AY
Table 16-378. Truth Table
AY
00
11

16.3.1.11 CLKINT

This macro routes an internal fabric signal to the global network.
Figure 16-177. CLKINT
Table 16-379. CLKINT I/O
InputOutput
AY
Table 16-380. CLKINT Truth Table
AY
00
11

16.3.1.12 GBR

Back-annotated macro that routes an internal fabric signal to global network.

Figure 16-178. GBR
Table 16-381. GBR
InputOutput
AnY
Table 16-382. Truth Table
AnY
00
11

16.3.1.13 CLKINT_PRESERVE

This Macro routes an internal fabric signal to the global network. It has the same functionality as CLKINT except that this clock always stays on the global clock network and will not be demoted during design implementation.
Figure 16-179. CLKINT_PRESERVE
Table 16-383. CLKINT_PRESERVE I/O
InputOutput
AY
Table 16-384. CLKINT_PRESERVE Truth Table
AY
00
11

16.3.1.14 GRESET

This Macro connects an I/O or route an internal fabric signal to the global reset network. The connection to the GRESET is hardened for radiation only if the driver is an I/O fixed at a package pin with GRESET in its function name. Routing an internal fabric signal through the GRESET macro is hardened by the radiation.

Figure 16-180. GRESET
Table 16-385. Truth Table
AY
00
11

16.3.1.15 RCLKINT

This Macro routes an internal fabric signal to a row global buffer, thus creating a local clock.

Figure 16-181. RCLKINT
Table 16-386. RCLKINT
InputOutput
AY
Table 16-387. Truth Table
AY
00
11

16.3.1.16 RGB

Back-annotated macro that routes an internal fabric signal to a row global buffer.

Figure 16-182. RGB.
Table 16-388. RGB
InputOutput
AnYL, YR
Table 16-389. Truth Table
AnYLYR
000
111

16.3.1.17 RGRESET

Macro used to route a triplicated fabric signal to a row global buffer and create a local reset. The three input bits must be driven by three separate logic cones replicating the paths from the source registers.

Figure 16-183. RGRESET
Table 16-390. Truth Table
A[2]A[1]A[0]Y
X000
0X00
00X0
X111
1X11
11X1

16.3.1.18 SLE

Sequential Logic Element.

Figure 16-184. Sequential Logic Element (SLE)
Table 16-391. Sequential Logic Element
InputOutput
NameFunctionName
DData inputQ
CLKClock input
ENActive-High CLK enable
ALnAsynchronous Load. This active-low signal either sets the register or clears the register depending on the value of ADn.
ADn1Static asynchronous load data. When ALn is active, Q goes to the complement of ADn.
SLnSynchronous load. This active-low signal either sets the register or clears the register depending on the value of SD, at the rising edge of the clock.
SD1Static synchronous load data. When SLn is active (that is, low), Q goes to the value of SD at the rising edge of CLK.
LAT1LAT is always tied to low. Q output is invalid when LAT=1.
Note:
  1. ADn, SD, and LAT are static signals defined at design time and need to be tied to 0 or 1.
Table 16-392. Truth Table
ALnADnLATCLKENSLnSDDQn+1
0ADnXXXXXX!ADn
1X0Not risingXXXXQn
1X0↑0XXXQn
1X0↑10SDXSD
1X0↑11XDD
XX1XXXXXInvalid

16.3.1.19 SLE_RT

Sequential Logic Element macro available only in post-layout netlist.

Figure 16-185. Sequential Logic Element (SLE)
Table 16-393.  Sequential Logic Element
InputOutput
NameFunctionQ
DData input
CLKClock input
ENActive High CLK enable
ALnAsynchronous Load. This active low signal either sets the register or clears the register depending on the value of ADn.
ADn1Static asynchronous load data. When ALn is active, Q goes to the complement of ADn.
SLnSynchronous load. This active low signal either sets the register or clears the register depending on the value of SD, at the rising edge of the clock.
SD1Static synchronous load data. When SLn is active (that is, low), Q goes to the value of SD at the rising edge of CLK.
DELEN1Enable Single-event Transient mitigation.
Note:
  1. ADn, SD, and DELEN are static signals defined at design time and need to be tied to 0 or 1.
Table 16-394. Truth Table
ALnADnCLKENSLnSDDQn+1
0ADnXXXXX!ADn
1XNot risingXXXXQn
1X↑0XXXQn
1X↑10SDXSD
1X↑11XDD

16.3.1.20 ARI1

The ARI1 macro is responsible for representing all arithmetic operations in the pre-layout phase.

Figure 16-186. ARI1
Table 16-395. ARI1
InputOutput
A, B, C, D, FCIY, S, FCO

The ARI1 cell has a 20 bit INIT string parameter that is used to configure its functionality. The interpretation of the 16 LSB of the INIT string is shown in the following table. F0 is the value of Y when A = 0 and F1 is the value of Y when A = 1.

Table 16-396. Interpretation of 16 LSB of the INIT String for ARI1
ADCBY
0000INIT[0]F0
0001INIT[1]
0010INIT[2]
0011INIT[3]
0100INIT[4]
0101INIT[5]
0110INIT[6]
0111INIT[7]
1000INIT[8]F1
1001INIT[9]
1010INIT[10]
1011INIT[11]
1100INIT[12]
1101INIT[13]
1110INIT[14]
1111INIT[15]
Table 16-397. Truth Table for S
YFCIS
000
011
101
110

ARI1 LOGIC

[Required-Cleanup]:

The 4 MSB of the INIT string controls the output of the carry bits. The carry is generated using carry propagation and generation bits, which are evaluated according to the following tables.

Table 16-398. ARI1 INIT[17:16] String Interpretation
INIT[17]INIT[16]G
000
01F0
101
11F1
Table 16-399. ARI1 INIT[19:18] String Interpretation
INIT[19]INIT[18]P
000
01Y
1X1
Table 16-400. FCO Truth Table
PGFCIFCO
0GXG
1XFCIFCI

16.3.1.21 ARI1_CC

The ARI1_CC macro is responsible for representing all arithmetic operations in the post-layout phase. It performs all the functions of the ARI1 macro except that it does not generate the Final Carry Out (FCO).
Note: FC1 and FC0 do not perform any functionalities.
Figure 16-187. ARI1_CC
Table 16-401. ARI1_CC
InputOutput
A, B, C, D, CCY, S, P, UB

The ARI1_CC cell has a 20-bit INIT string parameter that is used to configure its functionality. The interpretation of the 16 LSB of the INIT string is shown in the following table. F0 is the value of Y when A = 0 and F1 is the value of Y when A = 1. The following table shows the interpretation of 16 LSB of the INIT string for AR1_CC.

Table 16-402. Interpretation of 16 LSB of the INIT String for AR1_CC
ADCBY
0000INIT[0]F0
0001INIT[1]
0010INIT[2]
0011INIT[3]
0100INIT[4]
0101INIT[5]
0110INIT[6]
0111INIT[7]
1000INIT[8]F1
1001INIT[9]
1010INIT[10]
1011INIT[11]
1100INIT[12]
1101INIT[13]
1110INIT[14]
1111INIT[15]

The 4 MSB of the INIT string controls the output of the carry bits. The carry is generated using carry propagation and generation bits, which are evaluated according to the following tables.

Table 16-403. ARI1_CC INIT[17:16] String Interpretation
INIT[17]INIT[16]UB
001
01!F0
100
11!F1
Table 16-404. ARI1_CC INIT[19:18] String Interpretation
INIT[19]INIT[18]P
000
01Y
1X1

The equation of S is given by:

S=Y^CC

16.3.1.22 CC_CONFIG

The CC_CONFIG macro is responsible for generating the Carry bit for each ARI1_CC cell in the cluster.

Figure 16-188. CC_CONFIG
Table 16-405. CC_CONFIG
InputOutput
CI, P, UBCO, CC

CI and CO are the carry-in and carry-out, respectively, to the cell. The intermediate carry-bits are given by CC[11:0]. The functionality of the CC_CONFIG is basically evaluating CC using

CC[n] = !Px!UB+PxCC[n-1]

where CC[-1] is CI and CC[12] is CO.

Inside every cluster, there are 12 ARI1_CC cells and only one CC_CONFIG cell. The CC_CONFIG takes as input the P and UB outputs of each ARI1_CC cell in the cluster and generated the CC (carry-out bit), which is then fed to the next ARI1_CC cell in the cluster as the carry-in.

[Required-Cleanup]:

16.3.1.23 FCEND_BUFF

Buffer, driven by the FCO pin of the last macro in the Carry-Chain.

Figure 16-189. FCEND_BUFF
Table 16-406. FCEND_BUFF
InputOutput
AY
Table 16-407. Truth Table
AY
00
11

16.3.1.23.1 FCINT_BUFF

Name special Buffer, used to initialize the FCI pin of the first macro in the Carry-Chain.
Figure 16-190. FCINT_BUFF.
Table 16-408. FCINT_BUFF

Input

Output

A

Y

Table 16-409. Truth Table
AY
00
11

16.3.1.24 RCOSC_50MHZ

The RCOSC_50MHZ oscillator is an RC oscillator that provides a free-running clock of 50 MHz at CLKOUT.

Figure 16-191. RCOSC_50MHZ

16.3.1.26 SYSRESET

It is a special-purpose macro. The Output POWER_ON_RESET_N goes low at power-up and when DEVRST_N goes low.

Figure 16-192. SYSRESET
Table 16-410. SYSRESET
InputOutput
DEVRST_NPOWER_ON_RESET_N
Table 16-411. Truth Table
DEVRST_NPOWER_ON_RESET_N
00
11

16.3.1.27 SYSCTRL_RESET_STATUS

This special-purpose macro checks the status of the System Controller. The output port RESET_STATUS goes high when the System Controller is in reset. To enable this macro, select the "Enable System Controller Suspend Mode" option in the "Configure Programming Bitstream Settings" tool in Libero. After programming, the device enters System Controller Suspend Mode if TRSTB is tied low during power-up.
Important: This macro does not support simulation. To simulate the System Controller suspend mode, add the following pseudo-code to the simulation testbench:
  • At simulation time t = 0, set RESET_STATUS = 0.
  • 1.46 µs after observing POWER_ON_RESET_N = 1, set RESET_STATUS = 1 to indicate that the system controller has entered suspend mode.
Figure 16-193. SYSCTRL_RESET_STATUS

16.3.1.28 DFN1

D-Type Flip-Flop.
Figure 16-194. DFN1
Table 16-412. DFN1 I/O
InputOutput
D, CLKQ
Table 16-413. DFN1 Truth Table
CLKDQn+1
not RisingXQn
—DD

16.3.1.29 DFN1C0

D-Type Flip-Flop with active-low Clear.
Figure 16-195. DFN1C0
Table 16-414. DFN1C0 I/O
InputOutput
D, CLK, CLRQ
Table 16-415. DFN1C0 Truth Table
CLRCLKDQn+1
0XX0
1not RisingXQn
1—DD

16.3.1.30 DFN1E1

D-Type Flip-Flop with active high Enable.
Figure 16-196. DFN1E1
Table 16-416. DFN1E1 I/O
InputOutput
D, E, CLKQ
Table 16-417. DFN1E1 Truth Table
ECLKDQn+1
0XXQn
1not RisingXQn
1—DD

16.3.1.31 DFN1E1C0

D-Type Flip-Flop, with active-high Enable and active-low Clear.
Figure 16-197. DFN1E1C0
Table 16-418. DFN1E1C0 I/O
InputOutput
CLR, D, E, CLKQ
Table 16-419. DFN1E1C0 Truth Table
CLRECLKDQn+1
0XXX0
10XXQn
11not RisingXQn
11—DD

16.3.1.32 DFN1E1P0

D-Type Flip-Flop with active-high Enable and active-low Preset.

Figure 16-198. DFN1E1P0
Table 16-420. DFN1E1P0
InputOutput
D, E, PRE, CLKQ
Table 16-421. Truth Table
PREECLKDQn+1
0XXX1
10XXQn
11not RisingXQn
11↑DD

16.3.1.33 DFN1P0

D-Type Flip-Flop with active-Low Preset.
Figure 16-199. DFN1P0
Table 16-422. DFN1P0 I/O
InputOutput
D, PRE, CLKQ
Table 16-423. DFN1P0 Truth Table
PRECLKDQn+1
0XX1
1not RisingXQn
1—DD