1.1.3 Transmission
In the PLC & Go application, to transmit a message, it is only needed to call the
function APP_PLC_SendData() passing as parameters the pointer to the
data buffer and the data length. The function includes the length of the message to
transmit in the first two bytes of the data buffer so that, at the reception of the
message, it is possible to know the real length of the message.
Any message transmitted by the PLC_PHY module requires a header including some
transmission parameters. These parameters and the data are stored in the structure DRV_PLC_PHY_TRANSMISSION_OBJ.
The PLC & Go application only allow the configuration of some transmission parameters
related to the modulation. The rest of the parameters required to send a PLC message are
configured by default during the initialization stage in the function
APP_PLC_SetInitialConfiguration() in the state
APP_PLC_STATE_OPEN.
The function APP_PLC_SetInitialConfiguration() configures the
transmission parameters and stores the values in the structure.
Once the transmission is configured, the function APP_PLC_SendData()
prepares the data to be sent by PLC, storing the data in the transmission buffer
(appPlcTx.pDataTx) and indicating the length of the data buffer
(appPlcTx.pl360Tx.dataLength). When all the information is in the
transmission structure, the function DRV_PLC_PHY_Send() sends the PLC
message.
After sending the message to be transmitted to the PLC_PHY device, a TX data confirm
event is triggered indicating the result of the transmission. This event is managed by
the APP_PLC_DataCfmCb() callback function. This callback receives as
parameter a data structure of type DRV_PLC_PHY_TRANSMISSION_CFM_OBJ.
- Structure
DRV_PLC_PHY_TRANSMISSION_OBJ// ***************************************************************************** /* PRIME Transmission setup data Summary This struct includes all information to describe any transmissions. Remarks: None */ typedef struct __attribute__((packed, aligned(1))) { /* Pointer to data buffer to transmit */ uint8_t *pTransmitData; /* Instant when transmission has to start referred to 1us PHY counter */ uint32_t time; /* Length of the data to transmit in bytes */ uint16_t dataLength; /* Transmission Mode (absolute, relative, cancel, continuous). Constants above */ uint8_t mode; /* Attenuation level with which the message will be transmitted */ uint8_t attenuation; /* Forced transmission */ uint8_t forced; /* Buffer Id used for transmission */ DRV_PLC_PHY_BUFFER_ID bufferId; /* Scheme of Modulation */ DRV_PLC_PHY_SCH scheme; /* PRIME Frame type */ DRV_PLC_PHY_FRAME_TYPE frameType; } DRV_PLC_PHY_TRANSMISSION_OBJ;Transmission messages are composed using data structure
DRV_PLC_PHY_TRANSMISSION_OBJdefined indrv_plc_phy_comm.h.Where:pTransmitData: Pointer to the buffer containing the data to transmittime: Delay to send the message in ms referred to PLC_PHY internal timerdataLength: Length of the data buffer containing the data to transmitmode: Transmission modeuc_tx_mode Description TX_MODE_ABSOLUTE The message is sent at the specified time, referred to PL360 internal timer (1 us). Time defined in ul_tx_time.TX_MODE_RELATIVE The message is sent with a delay referred to the transmission request time. Delay defined in ul_tx_time.TX_MODE_PREAMBLE_CONTINUOUS Continuous transmission of the preamble. Used for testing. TX_MODE_SYMBOLS_CONTINUOUS Continuous transmission of a message. Used for testing. TX_MODE_CANCEL Cancels the ongoing transmission (started or programmed). attenuation: Attenuation level with which the message will be transmitted.bufferId: Buffer to store the transmission data. There are two available buffers. However, transmissions cannot be overlapped in time. In that case, TX_BUFFER_0 has priority.bufferId Description TX_BUFFER_0 First transmission buffer TX_BUFFER_1 Second transmission buffer modScheme: Modulation schemeuc_mod_scheme Value Description SCHEME_DBPSK 0 Differential BPSK SCHEME_DQPSK 1 Differential QPSK SCHEME_D8PSK 2 Differential 8PSK SCHEME_DBPSK_C 4 Differential BPSK Convolutional SCHEME_DQPSK_C 5 Differential QPSK Convolutional SCHEME_D8PSK_C 6 Differential 8PSK Convolutional SCHEME_R_DBPSK 12 Robust Differential BPSK SCHEME_R_DQPSK 13 Robust Differential QPSK frameType: Frame TypeframeType Value Description FRAME_TYPE_A 0 Frame Type A FRAME_TYPE_B 2 Frame Type B FRAME_TYPE_BC 3 Frame Type BC
- Structure
DRV_PLC_PHY_TRANSMISSION_CFM_OBJ// ***************************************************************************** /* PRIME Result of a transmission Summary This struct includes all information to describe any result of a previous transmission. Remarks: None */ typedef struct { /* Instant when frame transmission started referred to 1us PHY counter */ uint32_t time; /* RMS value emitted */ uint32_t rmsCalc; /* PRIME Frame type */ DRV_PLC_PHY_FRAME_TYPE frameType; /* Tx Result (see "TX Result values" above) */ DRV_PLC_PHY_TX_RESULT result; /* Buffer Id used for transmission */ DRV_PLC_PHY_BUFFER_ID bufferId; } DRV_PLC_PHY_TRANSMISSION_CFM_OBJ;The event returns one of the following transmission result values:// ***************************************************************************** /* PRIME Result values of a previous transmission Summary This list involves all available results from MCHP implementation Remarks: None */ typedef enum { /* Transmission result: already in process */ DRV_PLC_PHY_TX_RESULT_PROCESS = 0, /* Transmission result: end successfully */ DRV_PLC_PHY_TX_RESULT_SUCCESS = 1, /* Transmission result: invalid length error */ DRV_PLC_PHY_TX_RESULT_INV_LENGTH = 2, /* Transmission result: busy channel error */ DRV_PLC_PHY_TX_RESULT_BUSY_CH = 3, /* Transmission result: busy in transmission error */ DRV_PLC_PHY_TX_RESULT_BUSY_TX = 4, /* Transmission result: busy in reception error */ DRV_PLC_PHY_TX_RESULT_BUSY_RX = 5, /* Transmission result: invalid modulation scheme error */ DRV_PLC_PHY_TX_RESULT_INV_SCHEME = 6, /* Transmission result: timeout error */ DRV_PLC_PHY_TX_RESULT_TIMEOUT = 7, /* Transmission result: invalid buffer identifier error */ DRV_PLC_PHY_TX_RESULT_INV_BUFFER = 8, /* Transmission result: invalid PRIME Mode error */ DRV_PLC_PHY_TX_RESULT_INV_MODE = 9, /* Transmission result: invalid transmission mode */ DRV_PLC_PHY_TX_RESULT_INV_TX_MODE = 10, /* Transmission result: Transmission cancelled */ DRV_PLC_PHY_TX_RESULT_CANCELLED = 11, /* Transmission result: high temperature error */ DRV_PLC_PHY_TX_RESULT_HIGH_TEMP_120 = 12, /* Transmission result: high temperature warning */ DRV_PLC_PHY_TX_RESULT_HIGH_TEMP_110 = 13, /* Transmission result: No transmission ongoing */ DRV_PLC_PHY_TX_RESULT_NO_TX = 255, } DRV_PLC_PHY_TX_RESULT;