1.6.1 MCC Project Configuration

The following figure shows the MCC project graph of PRIME Service Dual Modem application for PIC32CXMTG-EK.

Figure 1-74. MCC Project Graph of PRIME Service Dual Modem for PIC32CXMTG-EK
  • Since it is an hybrid project, both PLC PHY and RF215 drivers are present. For PLC-only or RF-only projects, only one of them is needed.
  • The PLC PVDD Monitor service is needed to monitor the PVDD voltage of PL460 in order to disable PLC transmission in case the voltage is not in the expected range, to avoid PL460 damage. If the PVDD voltage is in the expected range, the PLC transmission is enabled.
  • The PLC PHY Coupling service is needed to configure the PLC transmission parameters for the selected transmission coupling branch.
  • The USI service is needed to send/receive messages through serial interface (UART/USB) to/from external device.
  • The Console and Debug system services are used to output information messages from Application and Log Report service.
  • The Time system service is required by both PLC PHY and RF215 drivers. It is used for timer control on PRIME Stack and Application (blink periodically the status LED).
  • The TRNG peripheral library is used by the Random service to generate random numbers, which is needed by the PRIME Stack. It is not mandatory due to the Random service can generate random numbers without it. However, if the used MCU has a TRNG peripheral, it is recommended to use it.
  • The Memory driver is used by the PRIME Firmware Upgrade service to manage the firmware images in the memory connected to the driver.
  • Crypto_v4 and wolfCrypt libraries are used by the Security service to perform cryptographic operations needed by the PRIME Stack and the Firmware Upgrade Service.
  • The PRIME STACK folder contains all the components needed by the PRIME Stack.
Figure 1-75. MCC Project Graph of PRIME STACK Folder
  • The PRIME SERVICES folder inside contains all the services needed by the PRIME Stack, except the Firmware Upgrade service, which needs to be in the root view due to its connection to the Memory driver. These services are required by the PRIME Stack.
Figure 1-76. MCC Project Graph of PRIME SERVICES Folder

The following figure shows the MCC configuration of the PRIME Stack.

Figure 1-77. PRIME Stack MCC Configuration
  • PRIME mode: It must be set to SN
  • Type of PRIME project: It must be set to application project
The following figure shows the MCC configuration of the PRIME PAL.
Figure 1-78. PRIME PAL MCC Configuration
  • Since it is an hybrid project, both PLC PHY and RF PHY interfaces are enabled. For PLC-only or RF-only projects, only one of them is needed. In a v1.3.6 project, it is possible to enable the Serial PHY interface, too.

For additional information about configuration of the PRIME Stack, the PRIME PAL and the PRIME Services, refer to the corresponding documentation.

PIC32CXMTG-EK Board Component

This component defines the board capabilities.

For this application, the following configuration is selected:
Figure 1-79. PIC32CXMTG-EK Component Configuration

Digital Interface

Green and Blue LEDs are selected, so corresponding PIOs are named and configured accordingly.

USB Debugger Interface

Virtual COM port interface is selected. This selection adds, links and automatically configures these components:
  • Console System Service
  • Flexcom0 Peripheral Library
    Figure 1-80. Console Configuration
    Figure 1-81. Flexcom0 Configuration
Note: Buffer sizes are increased manually for this application.

All related PIOs are automatically configured.

Xplained Pro Interface

PL460 Evaluation Kit at PHY level is selected to be connected to the Xplained Connector.

This selection automatically configures which pins of connector will be used, and in addition adds, links and automatically configures these components:
  • PLC PHY Driver
  • Flexcom5 Peripheral Library
  • ADC Peripheral Library
    Figure 1-82. PLC PHY Configuration
    Note: Thermal Monitor is manually enabled, and PRIME profile selected for this application.

    The PLC Coupling variant uses the default coupling stage of the evaluation kit (Multiband FCC + CENELEC-A for the PL460-EK). If other PLC band configuration is required, it can be easily modified.

    Figure 1-83. Flexcom5 Configuration
    Figure 1-84. ADC Configuration
    Note: Prescaler and Automatic Window Comparison are manually configured. For Comparison, only the Event Interrupt has to be enabled, the rest of parameters will be overwritten by the PVDD Monitor after initialization, so provided values in this configurator are not used.

All related PIOs are automatically configured.

Note: The PLC PHY Coupling component and the PLC PVDD Monitor component are not automatically added by the board component. They have been added to the project manually.

Additional Components

Apart from the previous components managed by PIC32CXMTG-EK component, others are required for this application:
  • Harmony Core Service
  • TRNG Peripheral Library
  • TIME System Service
  • TC0 Peripheral Library connected to TIME Service and configured as shown in the following figure:
    Figure 1-85. TC0 Configuration
  • USI Service configured as shown in the following figure:
    Figure 1-86. USI Configuration
  • Flexcom7 Peripheral Library connected to USI Service and configured by default
  • PLC PVDD Monitor Service connected to ADC Peripheral Library and configured as shown in the following figure:
    Figure 1-87. PVDD Monitor Configuration
  • PLC PHY Coupling automatically configured by the PLC PHY Driver
  • Memory Driver connected to SEFC0 and automatically configured by the Firmware Upgrade Service
  • RF215 Driver configured as shown in the following figure:
    Figure 1-88. RF215 Configuration
    In the pin configuration, configure the RF pins (all other pins are auto-configured by the SHD component):
    Figure 1-89. RF215 Pin Configuration
  • Flexcom3 Peripheral Library connected to RF215 Driver and automatically configured by it
  • Crypto_v4 and wolfCrypt Library, configured as shown in the following figure:
    Figure 1-90. wolfCrypt Library Configuration
  • Debug System Service connected to the Console System Service and configured as shown in the following figure:
    Figure 1-91. Debug Configuration