1.4.1 Application Example

Microchip PHY PLC & Go application is a point to multi-point chat application built on top of the state-of-the-art PHY layer of G3-PLC protocol.

This application example assumes that a host device (for example, a PC) is connected through a serial interface (UART, USB) to a Microchip evaluation kit acting as a PLC modem.

The figure below shows a block diagram of the PHY PLC & Go application.

Figure 1-37. PHY PLC & Go Block Diagram
The PLC & Go application interchanges data with the PC through a serial port using a terminal emulator (see Figure 1-38 where terminal emulator Tera Term is used). The settings of the serial port are:

When the terminal emulator is connected to the serial port and the first character is entered by the user, the PLC & Go application shows in the console some information about the hardware platform and the firmware running, and it waits for a PLC message to be sent/received or configuration request. The PLC message is sent when a carriage return character is entered. If the user enters the ASCII character 0x13 (‘CTRL+S’), a configuration menu is shown.

The PLC & Go application allows to:
  • Configure modulation type and modulation scheme used for transmission
  • Configure the frequency band (in case of using a Microchip evaluation board that supports several bands of transmission)
  • Enable/disable sleep mode (the STBY pin of the PLC device needs to be physically connected to a GPIO of the MCU host)

In addition, the application provides some information about the transmitted messages (length of the message) and the received messages (modulation type, modulation scheme, signal level and signal quality):

Figure 1-38. PHY PLC & Go Console
In the example application, the app_plc.c file contains:
  • PLC PHY initialization and configuration functions
  • Handlers for received messages, transmission and events
The following subsections explain in more detail the app_plc.c file.

The app_console.c file contains the chat application which communicates with the PC using the serial port.