1.7 SpaceWire Loopback Example
This example shows how to configure the SpaceWire peripheral to send and receive multiple packets. It uses multiple receive buffer to exercise in an optimize way the 3 states (NEXT, CURRENT, PREVIOUS) for packet reception.
Building The Application
The parent folder for all the MPLABX IDE projects for this application is given below:
- Application Path : apps\spw\spw_loopback\firmware
To build the application, refer to the table below and open the appropriate project file in MPLABX IDE.
| Project Name | Description |
|---|---|
| sam_rh707_ek.X | SAM RH707 Evaluation Kit board |
MPLAB Harmony Configurations
Refer to the MCC project graph for the components used and the respective configuration options.
Hardware Setup
- Project sam_rh707_ek.X
Hardware Used
- SAM RH707 Evaluation Kit
- SpaceWire cable
Hardware Setup
- Connect the USB port (USB DEBUG) on the board to the computer using a micro USB cable.
- If the board embedded debugger is not used, connect the debugger probe on DEBUG connector (J5).
- Connect the two SpaceWire link on the board to each other using a SpaceWire cable.
Note : This example can also be tested with SpaceWire links configured in TTL:
- Pin configuration must be modified in Harmony Configuration to set unused pin in an other function than SpaceWire.
- Evaluation kit board must be modified like described in the user guide.
- Connect the USB port (USB DEBUG) on the board to the computer using a micro USB cable.
Running The Application
Open the Terminal application (Ex.:Tera term) on the computer.
Connect to the Virtual COM port and configure the serial settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Build and Program the application using the MPLABX IDE.
See the following message in the console.
----------------------------------------------------------- SPW loopback example ----------------------------------------------------------- Wait for both SWP link switch to run state SPW Link in Run state TX time=3058836 us, for 25000000 bytes Effective rate=65 Mb/s Average RX process time = 39 us Rx sequence errors = 0 End of transfer