NET_PRES_TransBool Type
C
typedef bool (* NET_PRES_TransBool)(NET_PRES_SKT_HANDLE_T handle);
Returns
The result is passed directly through from the transport layer to the application. The meaning of the return is dependent on the transport function
Description
Transport Layer Boolean Function Pointer Prototype This function is called by the presentation layer when it accesses a function that takes no parameters apart from the socket handle and returns a boolean.
Preconditions
A socket needs to have been opened by NET_PRES_TransOpen.
Parameters
Parameters | Description |
---|---|
handle | The handle returned from NET_PRES_TransOpen. |