NET_PRES_TransIsPortDefaultSecured Type

C

typedef bool (* NET_PRES_TransIsPortDefaultSecured)(uint16_t port); 

Returns

  • true - The port is encrypted by default and the presentation layer will start negotiating encryption when it is connected.

  • false - The post is not encrypted by default.

Description

Presentation Layer Transport Layer Is Port Encrypted This function prototype is used by the presentation layer to determine if a port is encrypted by default or not when it is opened.

Preconditions

None.