NET_PRES_Status Function

C

SYS_STATUS NET_PRES_Status(SYS_MODULE_OBJ object); 

Returns

  • SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed

  • SYS_STATUS_UNINITIALIZED - Indicates the module has not been initialized

  • SYS_STATUS_BUSY - Indicates that the module is busy and can't accept operations

  • SYS_STATUS_ERROR - Indicates that there is a fatal error in the module

Description

This function provides the current status of the MPLAB Harmony Net Presentation Layer.

Remarks

None.

Preconditions

The NET_PRES_Initialize function must have been called before calling this function. Networking Presentation Layer Help Library Interface b) Socket Functions

Parameters

ParametersDescription
objectLayer object handle, returned from NET_PRES_Initialize