NET_PRES_SocketOptionsGet Function

C

bool NET_PRES_SocketOptionsGet(NET_PRES_SKT_HANDLE_T handle, NET_PRES_SKT_OPTION_TYPE option, void* optParam); 

Returns

  • true - Indicates success

  • false - Indicates failure

Description

Various options can be obtained at the socket level. This function calls directly to the transport layer's OptionGet function, if it exists.

Preconditions

A socket needs to have been opened by NET_PRES_SocketOpen.

Parameters

ParametersDescription
handleThe socket to set options for.
optionThe specific option to set, this is passed unaltered to the transport layer.
optParamThe option value, which is passed unaltered to the transport layer.