NET_PRES_SocketDiscard Function
C
uint16_t NET_PRES_SocketDiscard(NET_PRES_SKT_HANDLE_T handle);
Returns
The number of bytes that have been discarded from the RX buffer.
Description
This function calls the transport layer's discard function, if it exists.
Preconditions
A socket needs to have been opened by NET_PRES_SocketOpen
Parameters
Parameters | Description |
---|---|
handle | The presentation layer socket handle. |