1.5 Observing the Output on the Board and Serial Terminal
Press the Start button to open
Tera Term or PuTTY terminal application on the computer from the Start menu.
Select the required Serial Port and then click OK.Figure 1-21. Selection of Serial COM
Port
In the Tera Term Serial port setup
and connection dialog box, in the Speed box type or select the baud
rate to 115200.Figure 1-22. Setting the Baud
Rate
An LED (LED0) on the PIC32CM JH01 Curiosity Pro Development Evaluation Kit toggles
on a timeout basis and the default periodicity of the timeout is 500
milliseconds.
The LED toggling rate is displayed on
the Serial Terminal.
Press the switch SW0 on the PIC32CM
JH01 Curiosity Pro Evaluation Kit to change the default periodicity of the timeout
to one second.
Every subsequent pressing of the
switch SW0 on the PIC32CM JH01 Curiosity Pro Evaluation Kit changes the periodicity
of the timeout to 2 seconds, 4 seconds, 500 milliseconds, and back to 1 second in
cyclic order.Figure 1-23. LED Toggling Rate on a
Serial TerminalWhile the LED toggling rate on the Serial Terminal changes with every
subsequent switch press, observe the same change in the toggling rate of the LED0
on the evaluation kit.