2.4 IPE Modes
The IPE application operates in two modes:
- Production Mode – in which you can perform production programming operations. By default, the IPE is in Production Mode when it is launched. The Production Mode capabilities are set from the Advanced Mode menu discussed in 3.4.6 Production of this document.
- Advanced Mode – a feature-rich GUI interface in which you can view and change the settings for programming operations, and set up a production user interface for use on the manufacturing floor. To enable Advanced Mode, see 3.2 Setting Up the Programmer.