5 Revision History
Revision A (December 2013)
Initial release of this document.
Revision B (August 2015)
Modified “Software Installation Requirements”. The IPE is now a separate installation than the MPLAB X IDE.
Modified the description of Production Mode.
In the General Setup chapter:
- Added information on new features: Recently Used option in the Family list of devices and Creating Desktop Shortcuts.
- Added information on Preserve Memory options.
- Added notes regarding MPLAB PM3 programmer environment files.
- Added a note in the description of the Allow Import Hex file option.
- Added information regarding using the MPLAB PM3 programmer with the option Allow “Communication” under Settings menu.
- Added Special Memory Regions information.
In The MPLAB IPE Reference chapter:
- Added a note regarding the File>Import>Hex option.
Revision C (March 2017)
- Added Note with location of the Readme file for MPLAB IPE in “Software Installation Requirements”.
- Added a “Staying Logged In” topic to the Advanced Mode Login section.
- Updated memory range descriptions.
- Updated environment settings options.
- Revised “SQTP” section and added sections for using SQTP with MPLAB PM3 and with PIC32 devices.
- Added new SQTP setting.
- Updated field descriptions to the main IPE window.
- Added new Read Device ID option to the View menu.
- Added new settings menu command for saving firmware into SD card and added a revised information to “Save Firmware into PM3 SD Card”.
Revision D (June 2018)
- In the Preface, added compatibility note that this document reflects the changes as of MPLAB X IDE v4.20 or greater.
- Multiple updates throughout to reflect changes made to the program for the NetBeans platform. Added Tools and Windows menus, updated graphics, text, and menu options.
Revision E (April 2020)
- Entire document has been reformatted and renumbered.
- In the Preface, added compatibility note that this document reflects the changes as of MPLAB X IDE v5.40 or greater.
- Replaced screen for Select Applications Dialog in the “Software Installation Requirements” section.
- Removed the “Feature Matrix” section.
- Added a new heading for “Multiple Instances of IPE” in Launching the MPLAB IPE Application section.
- Replaced screen for Advanced Mode Login and added screen for Change Password and Forgot Password dialogs.
- Updated Production Settings table.
- Updated Special Settings table, added information for tool and device packs and other options including Programmer-To-Go, JTAG, etc. Also removed PM3 program speed option and screen.
Revision F (December 2021)
- Updated Tools menu to add options for Manage Network Tools, Download Plugins and Hardware Tool Emergency Boot Firmware Recovery.
- Added support information for MPLAB ICE 4 Emulator.
Revision G (November 2022)
- Updated Tools menu to add Packs Manager feature.
- Added screenshots and steps for navigating the Packs menu and Pack manager window.
- Updated Window menu to document OTP fuse support.
- Updated Settings menu to move options from Program to Programming.
Revision H (April 2023)
Under Advanced Mode Settings:
- Updated Programming Tools Supported to reflect Gen 5 tools.
- Updated Special Settings section to reflect Erase All Before Program option.
- Updated Special Settings section to reflect Browse PTG Image functionality.
- Added section about Python script-enabled devices.
Revision I (February 2025)
- Updated section 2.3 Programming Tools Supported to reflect MPLAB ® PICKit Basic In-Circuit Debugger
- Updated Settings table in section 3.4.7 Settings to include Bluetooth functionality