4 LIN Responder Basic Demo

This section provides a basic LIN communication between an 8-bit Curiosity Nano (CNANO) as Responder and the APG LIN Serial Analyzer as Commander.

4.1 Hardware Setup

The following hardware tools are used:
Note:
  1. Refer to 8-bit Curiosity Nano Boards for the complete set of supported CNANO boards.

Configure the hardware as shown below. Plug the ATA663254 click to the mikroBUS™ socket 1 of the CNANO base.

Figure 4-1. Hardware Configuration

An example setup is shown below. The CNANO board and LIN Serial Analyzer are connected to the PC via USB. The LIN Serial Analyzer is powered by a 9V supply.

Figure 4-2. Hardware Setup

4.2 Software Environment

This demo is compatible with both the MPLAB® X IDE and the Visual Studio Code® (VS Code®) environment.

For new projects, it is recommended to download and install the following tools:

To evaluate with MPLAB X IDE, run the project with the following:

Install the LIN Serial Analyzer v3.0.0 before proceeding.

Note: Always check for the latest available version of software tools.

4.3 Demo Network

This demo utilizes the readily-available LED (LED0) and push button switch (SW0) from the CNANO board.

Table 4-1. Frames, Signals and Nodes Definition
FrameIDLength (Bytes)SignalsPublisherSubscriber
LED_Blink0x002Bit[15:0] Blink_PeriodLIN AnalyzerCNANO
Switch_Status0x011Bit[0] SW_StateCNANOLIN Analyzer
Error_Status0x3B1Bit[0] CNANO_ErrBitCNANOLIN Analyzer

Blink_Period represents the 16-bit toggle period of LED0 in milliseconds. SW_State returns the status of SW0 while CNANO_ErrBit is the 1-bit response error signal required in LIN 2.x.

4.4 MCC Melody Configuration

The following instructions will walk the user through the steps for setting up a LIN Responder node’s peripherals, frames and signals.

Note: The Melody window appearance might be slightly different between MPLAB X IDE and VS Code, but all steps defined in the next sections are applicable to both.

4.4.1 Loading the Library

  • To check if the latest version of the library is installed, click the Content Manager button at the upper left part of the Melody window. This will open the MCC Content Manager tab.
  • Under the Content Libraries tab, go to Libraries>LIN>LIN Responder. Select the latest version and hit the Apply button. The Melody windows will automatically refresh.
  • Under Device Resources, select Libraries>LIN>LIN Responder. The LIN Responder can now be found under Project Resources.

The user has two options from here: manually configure the node attributes and frames, or use an LDF. To configure without an LDF, continue with Manual Configuration. To configure with an LDF, proceed to Configuration With LDF .

4.4.2 Manual Configuration (No LDF)

  • Click the LIN Responder block in the Application Builder tab. This can also be done by going to Project Resources>Libraries>LIN>LIN Responder.
  • In the LIN Responder GUI, go to the Frames tab and add the following signals and frames:

    Figure 4-3. Manual Frames Configuration
  • Go to the General tab and configure the fields as shown below

    Figure 4-4. Manual Node Configuration

4.4.3 Configuration With LDF

If manual configuration has already been done, skip this section and proceed to Frame Processor Configuration.

  • Copy and paste the below LDF to a text editor. Save the file with an .ldf extension.
    LIN_description_file;
    LIN_protocol_version = "2.2";
    LIN_language_version = "2.2";
    LIN_speed = 19.2 kbps;
    
    Nodes {
      Master: LIN_Analyzer, 1 ms, 0 ms ;
      Slaves: CNANO ;
    }
    
    Signals {
      LED_Blink_Period: 16, 0, LIN_Analyzer, CNANO ;
      SW_State: 1, 0, CNANO, LIN_Analyzer ;
      CNANO_ErrBit: 1, 0, CNANO, LIN_Analyzer ;
    }
    
    Frames {
      LED_Blink: 0, LIN_Analyzer, 2 {
        LED_Blink_Period, 0 ;
      }
      Switch_Status: 1, CNANO, 1 {
        SW_State, 0 ;
      }
      Error_Status: 59, CNANO, 1 {
        CNANO_ErrBit, 0 ;
      }
    }
    
    Node_attributes {
      CNANO{
        LIN_protocol = "2.2" ;
        configured_NAD = 0xFF ;
        initial_NAD = 0xFF ;
        product_id = 0x0, 0x0, 255 ;
        response_error = CNANO_ErrBit ;
        P2_min = 50 ms ;
        ST_min = 0 ms ;
        N_As_timeout = 1000 ms ;
        N_Cr_timeout = 1000 ms ;
        configurable_frames {
          LED_Blink ;
          Switch_Status ;
          Error_Status ;
        }
      }
    }
    
    Schedule_tables {
     Demo_Sched {
        LED_Blink delay 5 ms ;
        Switch_Status delay 10 ms ;
        Error_Status delay 10 ms ;
      }
    }
  • Click the LIN Responder block in the Application Builder to open the LIN Responder configuration window. This can also be done by going to Project Resources>Libraries>LIN>LIN Responder.
  • Enable Use LDF
  • Click Select File and load the LDF

    Figure 4-5. Node Settings Example Using LDF
  • Select “CNANO” as the Responder Node. The Node Attributes will be automatically populated.
  • The Frames tab will display as shown below

    Figure 4-6. Frames Configuration With LDF

4.4.4 Frame Processor Configuration

  • In the General tab, configure the Frame Processor mode to “Non-blocking”

    Figure 4-7. Frame Processor Configuration

4.4.5 UART and Timer Configuration

  • Select EUSART1 as the LIN Responder’s UART and set the baud rate to 19200. The baud rate is already filled in and uneditable when an LDF is loaded.
  • Select TMR0 as the Timer

    Figure 4-8. LIN UART and Timer Configuration

4.4.6 Pins Configuration

  • Go to the Pin Grid View tab and configure the EUSART1 pins: TX1 to RC2 and RX1 to RC3

  • Set RD4 and RE0 as GPIO output pins and RE2 as an input pin
    Figure 4-9. Pin Grid View
  • Click the Pins block from the Application Builder. Configure the pins as shown below.

    Figure 4-10. Pin Configuration

4.4.7 Adding Timer for LED Blink

Add a 16-bit timer to generate an interrupt every 1 ms period. This resource will be used for blinking the CNANO LED and is different from the configured LIN Responder’s timer.

  • Load Timer1 from Device Resources
  • Under Hardware Settings, enable Timer and 16-Bit Read/Write mode
  • Set the Requested Period to 1 ms and enable TMR Interrupt

    Figure 4-11. LED Blink Timer Configuration

4.4.8 Generating the Code

  • Go to the Notifications tab and address any warnings. Take note of the Hints.
  • Hit the Generate button next to Project Resources

4.4.9 Adding the Application Code

  • After a successful generation, open the main.c file and add the following code:
    #include "mcc_generated_files/system/system.h"
    
    /*
        Main application
     */
    
    void LED_BlinkPeriodSet(void);
    void SW_StatusRead(void);
    void LED_Toggle(void);
    void Timer_Stop(void);
    
    uint16_t blinkPeriod = 0;
    uint16_t counter = 0;
    
    int main(void)
    {
        SYSTEM_Initialize();
    
        // Enable the Global Interrupts 
        INTERRUPT_GlobalInterruptEnable();
    
        // Enable the Peripheral Interrupts 
        INTERRUPT_PeripheralInterruptEnable();
    
        LEDBLINK_AppCallbackRegister(LED_BlinkPeriodSet);
        LINRESP_ShortRespErrCallbackRegister(Timer_Stop);
        Timer1_OverflowCallbackRegister(LED_Toggle);
    
        while (1)
        {
            SW_StatusRead(); 
            // Uncomment the following line when the LIN frame processor is configured in blocking mode:
            // LINRESP_Handler(); 
        }
    }
    
    void LED_BlinkPeriodSet(void)
    {
        Timer1_Stop();
        
        blinkPeriod = l_u16_rd_LED_Blink_Period();
        counter = 0;
        
        Timer1_CounterSet(0);
        Timer1_Start();
    }
    
    void LED_Toggle(void)
    {
        if(++counter == blinkPeriod)
        {
            LED0_Toggle();
            counter = 0;
        }
    }
    
    void SW_StatusRead(void)
    {
        if (SW0_GetValue() == HIGH)
        {
            l_bool_wr_SW_State(0);
        }
        else
        {
            l_bool_wr_SW_State(1);
        }
    }
    
    void Timer_Stop(void)
    {
        Timer1_Stop();
    }
    
  • Do a Clean and Build

  • If there are no build issues, hit Make and Program Device

4.5 LIN Analyzer Setup

  • Open the LIN Serial Analyzer software
  • Go to Tools and Options>Configure LIN Analyzer and set the baud rate to 19200

    Figure 4-12. LIN Analyzer Configuration
  • Hit the Connect and Initialize LIN Analyzer button before closing the pop-up window. A “LIN Analyzer initialized” status is displayed in the footer of the main window.
  • In the main UI, add the following LIN frames and set the Checksum Type to “Enhanced”

    Figure 4-13. LIN Analyzer Frames
  • Select the frames to be sent and click the Send Once button

4.6 Demo Output

A sample output of the LIN Serial Analyzer is shown below. The LIN Analyzer window displays the Protected Identifier (PID) of each frame on the Frame ID column.

Figure 4-14. LIN Serial Analyzer Output

LED Blink Frame (ID = 0x00, PID = 0x80)

Byte 0 and Byte 1 of this frame correspond to the lower and upper byte the LED blink period with a time base of 1 ms.

Changing the data from [FF 00] to [E8 03], which are equivalent to 0x00FF and 0x03E8 in 16-bit hex, respectively, will update the Responder node’s LED blink period from ~255 ms to ~1000 ms. 0x00FF is equivalent to 255 in decimal while 0x03E8 is equal to 1000.

Figure 4-15. Controlling the LED Blink Period

Switch Status Frame (ID = 0x01, PID = 0xC1)

This frame includes a Boolean signal corresponding to the state of the CNANO’s on-board switch. Bit 0 of the frame’s Byte 0 is set to ‘1’ when the button is pressed and ‘0’ if released.

Error Status Frame (ID = 0x3B, PID = 0xFB)

This frame includes a Boolean signal for the error bit required for LIN 2.x. Bit 0 of the frame’s Byte 0 is set to ‘1’ when the previous frame includes an error.

In the above example, a Response Too Short error was introduced by sending an incomplete frame with PID 0x80. The Responder node expects two bytes of data and the checksum byte. Since the Commander transmitted only one data byte and the checksum byte within the time-out period, the Responder flagged this frame as erratic and automatically set the error signal bit.

The application program stops the LED blink timer when a Response Too Short error is detected.

Figure 4-16. Response Too Short Error Detection