4.1.6 Creating a New Project

Figure 4-5. MPLAB X IDE Start-up Screen
  1. To create a new project, open MPLAB X IDE and click File>New Project
    Figure 4-6. New Project
  2. In the “New Project” pop-up, click Microchip Embedded>Application Project(s)>Next
    Figure 4-7. Choose Project
  3. In Select Device window, select the device ATSAME54P20A and click Next.
    Figure 4-8. Select Device
  4. In Select Compiler window, select the latest compiler and click Next.
    Figure 4-9. Select Compiler
  5. In Select Project Name and Folder window, enter the project name and select the project location, and click Finish.
    Figure 4-10. Select Project Name and Folder
  6. Now MPLAB X Code Configurator Content Manager will be launched automatically.
    1. Click Finish.
      Figure 4-11. MCC Required Content
    2. Under Device Resources, click the Content Manager
      Figure 4-12. MCC Content Manager
    3. In the next window, select the below mentioned versions of repositories and click Apply.
      • core (v3.13.5 or above)
      • bsp (v3.21.0 or above)
      • wireless_apps_rnwf (v3.0.0)
      • wireless_system_rnwf (v3.0.0)
        Figure 4-13. MCC Components
      • Click Apply
        Figure 4-14. MCC Apply
    4. The MCC content manager will start downloading the repositories.
      Figure 4-15. Downloaded Repositories